cancel
Showing results for 
Search instead for 
Did you mean: 

PA1 EXTERNAL INTERRUPT ISSUE

Khansokhua
Associate

Hello,

STM32CubedIDE, STM407G DISC1 BOARD

     I am trying to trigger an external interrupt by using a button connected to PA1 pin. 

My configurations are below;

  1-) I enabled 7.bit in NVIC_ISER register.   IRQN_EXTI0 is enabled

  2-) I enabled  GPIOAEN  in RCC register.    GPIOA  clock is enabled.

  3-)  I wrote  '1' into the  TR1 in EXTI> RTRS register for RISING EDGE. 

  4-)  I enabled SYSCFG clock.

  5-)  Although the reset value is already '0'(which is corresponding to A Port) 

         for  SYSCFG_EXTICR1> EXTI1, I wrote '0' again for Port A and pin 1(EXTI1)

   6-) I set EXTI>IMR> MR1 bit in the register for not masking the line 1( due to being 1.pin )

   7-) Other pin configurations are, Pull-Down, High-Speed and Push-Pull for OTYPE

I succeed in making it work for PA0 and PB0 external interrupts individually.I debugged each step and it seems everything is fine. I suspect due to I use first pin, I am missing something here.I haven't figured it out yet. However, PA0 and PA1 share most register common.Only difference could be the MR bits but I have checked  them several times.

For better understanding, I tried to capture the high logic with a single LED using PA1 button, after I configurated it identically as in the above.Result is positive, I can capture it is able to be high but cannot trigger interrupt. What am I missing? I am looking forward to handle the issue. Thank you for your assistance. 

Respects Khansokhua

1 ACCEPTED SOLUTION

Accepted Solutions

The 0..15 relate to the pin# in ONE bank, PA13 would dump into EXTI15_10_IRQHandler

Perhaps review the diagram/illustration in the Reference Manual (RM0090) describing HOW things work.

 

                DCD     EXTI0_IRQHandler                  ; EXTI Line0
                DCD     EXTI1_IRQHandler                  ; EXTI Line1
                DCD     EXTI2_IRQHandler                  ; EXTI Line2
                DCD     EXTI3_IRQHandler                  ; EXTI Line3
                DCD     EXTI4_IRQHandler                  ; EXTI Line4
...
                DCD     EXTI9_5_IRQHandler                ; External Line[9:5]s
...
                DCD     EXTI15_10_IRQHandler              ; External Line[15:10]s

 

You'd generally put the higher priority ones on lower pin#, but it's a bit of a wash, especially with the layers of inefficiency HAL/CUBE add.

Avoid doing too much in IRQ / Callback context, do what you need quickly and leave.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

13 REPLIES 13
SofLit
ST Employee

Hello @Khansokhua and welcome to the community,

I suggest you starting by programming with HAL and especially inspiring from this example:

https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F4-Discovery/Examples/GPIO/GPIO_EXTI

If it does work you can move forward and go with programming doing direct access to the registers inspiring from the HAL implementation.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Khansokhua
Associate

Thank you! @SofLit I am also planning to use HAL. However, I need some clarification for my current position right now. What do you think the problem is here?

Bit 0 is 0x01

Bit 1 is 0x02

EXTI1_IRQHandler ; EXTI Line1

void EXTILine1_Config(void)
{
  GPIO_InitTypeDef GPIO_InitStructure = {0};

  /* Enable GPIOA clock */
  __HAL_RCC_GPIOA_CLK_ENABLE();
  
  /* Configure PA1 pin as input floating */
  GPIO_InitStructure.Mode = GPIO_MODE_IT_FALLING;
  GPIO_InitStructure.Pull = GPIO_NOPULL;
  GPIO_InitStructure.Pin = GPIO_PIN_1;
  HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);

  /* Enable and set EXTI Line1 Interrupt to the lowest priority */
  HAL_NVIC_SetPriority(EXTI1_IRQn, 2, 0);
  HAL_NVIC_EnableIRQ(EXTI1_IRQn);
}

void EXTI1_IRQHandler(void)
{
  HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_1);
}
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

You just tell by text what you did and this is not efficient. You need to share your code.

And again, please inspire from the HAL implementation to know how to implement a correct sequence of the direct access to the register.

@Tesla DeLorean gave you an example of using HAL.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for your answer @Tesla DeLorean . I use EXTI0_IRQHandler, for PA1.

I thought, 0-3 pins EXTI0,  4-7  EXTI1 8-11 EXTI2, 12-15 EXTI3.

Here my question, if I need to use EXTI1_IRQHandler  for PA1 external interrupt.

Then which handler do I need to use for (let's say) PA13 external interrupt? What is the rule here?

and If I have to use EXTI1_IRQHandler for PA1. I guess I also need to enable IRQN_EXTI1. Then from starting previous example how do I need to enable corresponding bit in ISER? 

It seems I mixed some terms up.I will send the code for better clarity.You are absolutely right @SofLit 

So you can assist me more efficiently.

Khansokhua
Associate

 

void EXTI0_IRQHandler(void)
{

	if(EXTI->PR & (1u << 0))
	{
		GPIOD->ODR |= (1u << 13);
		EXTI_SET_PR_0();
	}
	else if(EXTI->PR & (1u << 1))
	{
		GPIOD->ODR |= (1u << 13);
		EXTI_SET_PR_1();
	}

}
 
int main(void)
{
				GPIO_Handle_t EXTI_A0 = {  .PORTNAME = GPIOA,
						 	 	 	   .PINCONF.PIN = GPIO_PIN_0,
									   .PINCONF.MODE = GPIO_MODE_INT_RISING,
									   .PINCONF.OTYPE = GPIO_OTYPE_PP,
									   .PINCONF.OSPEED = GPIO_OSPEED_HIGH,
									   .PINCONF.PUPD = GPIO_PUPD_PD,
									   .PINCONF.AF = GPIO_AF_NO

				 	 	 	 	 	 };
				GPIO_Handle_t EXTI_A1 = {  .PORTNAME = GPIOA,
									 	   .PINCONF.PIN = GPIO_PIN_1,
										   .PINCONF.MODE = GPIO_MODE_INT_RISING,
										   .PINCONF.OTYPE = GPIO_OTYPE_PP,
										   .PINCONF.OSPEED = GPIO_OSPEED_HIGH,
										   .PINCONF.PUPD = GPIO_PUPD_NO,
										   .PINCONF.AF = GPIO_AF_NO

								 	 	 	 	 	 };

				GPIO_Handle_t orange_LED = {  			   .PORTNAME = GPIOD,
														   .PINCONF.PIN = LED_ORANGE,
														   .PINCONF.MODE = GPIO_MODE_OUTPUT,
														   .PINCONF.OTYPE = GPIO_OTYPE_PP,
														   .PINCONF.OSPEED = GPIO_OSPEED_HIGH,
														   .PINCONF.PUPD = GPIO_PUPD_PD	,
														   .PINCONF.AF = GPIO_AF_NO

										   };  
          gpioInit(&orange_LED);
nvicInterruptEnable(IRQN_EXTI0);
             gpioInit(&EXTI_A1); // gpioInit includes SYSCFG, IMR etc configuration
             gpioInit(&EXTI_A0); //  A0 works fine
     while(1)
     {
     }
}

 


@Khansokhua wrote:

Here my question, if I need to use EXTI1_IRQHandler  for PA1 external interrupt.

Then which handler do I need to use for (let's say) PA13 external interrupt? What is the rule here?.


It depend on the product:

but the rule for PYn and EXTIm_IRQHandler: where Y is the port and n is the pin number, m the available EXTI line number or range.

So n needs to be = m if m is a value or at least n needs to be in the range of m.

Example for STM32F405 product:

If you need to use PA7 as source of EXTI interrupt you need to use 

EXTI9_5_IRQHandler(): 7 is in the range of [5..9]

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I can only see five handler in start-up file for STM407.

  .word	EXTI0_IRQHandler             			/* EXTI Line0 interrupt                                               */
  .word	EXTI1_IRQHandler             			/* EXTI Line1 interrupt                                               */
  .word	EXTI2_IRQHandler             			/* EXTI Line2 interrupt                                               */
  .word	EXTI3_IRQHandler             			/* EXTI Line3 interrupt                                               */
  .word	EXTI4_IRQHandler             			/* EXTI Line4 interrupt                                               */

 

The 0..15 relate to the pin# in ONE bank, PA13 would dump into EXTI15_10_IRQHandler

Perhaps review the diagram/illustration in the Reference Manual (RM0090) describing HOW things work.

 

                DCD     EXTI0_IRQHandler                  ; EXTI Line0
                DCD     EXTI1_IRQHandler                  ; EXTI Line1
                DCD     EXTI2_IRQHandler                  ; EXTI Line2
                DCD     EXTI3_IRQHandler                  ; EXTI Line3
                DCD     EXTI4_IRQHandler                  ; EXTI Line4
...
                DCD     EXTI9_5_IRQHandler                ; External Line[9:5]s
...
                DCD     EXTI15_10_IRQHandler              ; External Line[15:10]s

 

You'd generally put the higher priority ones on lower pin#, but it's a bit of a wash, especially with the layers of inefficiency HAL/CUBE add.

Avoid doing too much in IRQ / Callback context, do what you need quickly and leave.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..