2024-06-13
03:11 AM
- last edited on
2024-06-14
05:38 AM
by
Lina_DABASINSKA
Hi can I leave PDR_ON pin as No Connect for STM32F46x LQFP208 and VBAT connected to VDD. Not really using the Internal reset function.
2024-06-13 12:29 PM
PDR_ON does not have any internal pullup or pulldown, so it must be connected to either VDD or VSS.
> Not really using the Internal reset function.
So, do you have an external reset chip to rely on?
JW
PS. Don't hijack threads, especially if they are 12 years old. Start your own and discuss there.