2016-07-06 05:54 PM
Hi,I have one
nucleoF411
+IKS01A1
kit.I follow the steps ofIKS01A1
quick start guides().However, After I connected the board to computer and finished the steps, there is no response. I check the device manager in windows Os and find that the driver of the com port is not properly installed,as depicted in fig.I have tried with32bits
and 64 bitswin7
computers , however , it doesn't work. Should I install theVCP
driver? Any hints would be very grateful, thank you.2016-07-07 09:26 AM
The drivers and firmware included in the ST-LINK Utilities v3.9.0 should be sufficient to connect to the board and provide a VCP interface.
2016-07-07 06:55 PM
Many thanks clive1, the problem has been worked out , the vcp driver is installed with the pack. The pack is only tried with 64bits win7, and it works.
________________ Attachments : 1.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzxY&d=%2Fa%2F0X0000000bRR%2FyHjBlsezx95p2wL7EUQMbD2MpoxrWC225lxruVx.w_g&asPdf=falsemdmcpq.inf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzxT&d=%2Fa%2F0X0000000bRT%2F1SJz.xmyTPqn5JIL7UcTwYxrBU75S6YBtfoqAkhM7sc&asPdf=falseusbser.sys : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzx9&d=%2Fa%2F0X0000000bRQ%2Fgo9W_ieT2ZCtbwxcH82AQXmVDmbQyxPUhqBXUBMnZxs&asPdf=false