2021-02-07 09:15 AM
hello,
I try to use the AD9834 with the nucleo L476RG and I have some issue.
I use Spi 1 , send that I think good, but it's not work.
here are my code, I hope someone can help.
thanks and sorry for my english
int PINSW = 1;
//int led = GPIO_PIN_5;
int AD_reset = GPIO_PIN_15;
int AD_SDA = GPIO_PIN_14;
int AD_SLK = GPIO_PIN_13;
int AD_FSY = GPIO_PIN_12;
int AD_CSK = GPIO_PIN_5;
uint8_t spitx[2];
void AD9834_Reset(int value){
if(PINSW){
if(value) HAL_GPIO_WritePin(GPIOB, AD_reset,1);
else HAL_GPIO_WritePin(GPIOB, AD_reset,0);
}else{
if(value) AD9834_CONTROL |= 0x0100;
else AD9834_CONTROL &= ~0x0100;
//AD9834_SendWord(AD9834_CONTROL);
}
}
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_SPI2_Init();
MX_SPI1_Init();
/* USER CODE BEGIN 2 */
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
//AD9834_Reset(0);
HAL_Delay(2000);
//AD9834_Reset(1);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0x00;
spitx[1]=0x21;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0xC7;
spitx[1]=0x50;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
//freq
spitx[0]=0xFB;
spitx[1]=0x0E;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0x00;
spitx[1]=0x40;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0x00;
spitx[1]=0x00;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0x00;
spitx[1]=0xC0;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0x00;
spitx[1]=0x00;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0x00;
spitx[1]=0x20;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
//HAL_GPIO_TogglePin(GPIOA, led);
// HAL_GPIO_TogglePin(GPIOB, AD_FSY);
//spitx[1]=0x00;
//HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
// HAL_Delay(2000);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 10;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief SPI1 Initialization Function
* @param None
* @retval None
*/
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_16BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
/**
* @brief SPI2 Initialization Function
* @param None
* @retval None
*/
static void MX_SPI2_Init(void)
{
/* USER CODE BEGIN SPI2_Init 0 */
/* USER CODE END SPI2_Init 0 */
/* USER CODE BEGIN SPI2_Init 1 */
/* USER CODE END SPI2_Init 1 */
/* SPI2 parameter configuration*/
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_16BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI2_Init 2 */
/* USER CODE END SPI2_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @param None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
/*Configure GPIO pin : B1_Pin */
GPIO_InitStruct.Pin = B1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
2021-02-07 03:59 PM
o
2021-02-09 12:19 AM
Hello @Seth1er and welcome to the STM32 Community 😊 ,
Please share your ioc file and more details to help you solve your issue :
Which version of CubeL4 and CubeMx are you using ?
In the debug, where the code hangs/stop ? Do you get an error message ?
Imen
2021-02-09 02:20 AM
hello,
here are the ioc file.
cubeide version :
Version: 1.5.1
Build: 9029_20201210_1234 (UTC)
I don't know what is CubeL4 sorry. if it's the nucle version, i don't know how to check.
In fact I don't have any arror message. the code is load, I send some data on the SPI to the AD9834 but I don't have any signal.
after some try I have one success, with code below( with luck) I have a 6,25MHz signal. I don't understand why, because it doesn't correspond to the 9834 formula.
If I try an other value, I don't have any signal.
I don't know if it's an SPI issue, a sequence issue .
I don't found any exemple on net between SMT32 and AD9834. a lot with arduino, but all exemple don't use the SPI, they make they own one.
I hope someone can help me. it seem to be easy but i can't .
The AD9834 is on a "eval" board with the clk inside a 75MHz.
BR,
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0x00;
spitx[1]=0x21;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
spitx[0]=0xC7;
spitx[1]=0x50;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 0);
HAL_Delay(100);
//freq
spitx[0]=0xFB;
spitx[1]=0x0E;
HAL_SPI_Transmit(&hspi1, spitx, 1, 100);
HAL_Delay(100);
HAL_GPIO_WritePin(GPIOB, AD_FSY, 1);
2021-02-10 01:57 AM
just a up,
if someone can help me on this please. or give me a simple code to set a freq with STM32 and AD9834, I will understand
BR