2020-11-30 9:54 PM
Hello,
When I activate ADC channel I'm getting 2035 value without any connection from ADC channels, I changed several channel
HAL_ADC_Start(&hadc);
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
raw = HAL_ADC_GetValue(&hadc);
// Convert to string and print
sprintf(msg, "%hu\r\n", raw);
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
2020-11-30 10:12 PM
That is OK, unconnected ADC input doesn't mean there is 0V on it.
Connect input voltage. Observe required impedance of the voltage source versus sample time, see datasheet.
JW
2020-11-30 10:22 PM
I thought there is fail on MCU after I tried same code on F4Disco Board when ADC unconnect I got 0 value
Do you mean float voltage ?
Thanks,
2020-11-30 10:36 PM
I pulled down ADC channel with 10K resistor , there is no affect I couldn't find graph on datasheet
2020-11-30 11:30 PM
Did you check external connections of the associated GPIO pin on the F030 Nucleo board ?
2020-12-01 12:26 AM
Yes of course , I tried several ADC channels , When I activate channel 1,65V appear on pin
Deactivate channels are 0V
2020-12-01 1:11 AM
> I pulled down ADC channel with 10K resistor , ...
Connect it directly to GND - if you are sure there are no other external connections.
Any pull-up/pull-down resistor should be less than the recommended ADC input impedance.
I do not trust the Cube/HAL code either.
Did you check the GPIO/ADC register settings, and the raw conversion results ?
2020-12-01 1:30 AM
When I connect to ADC VCC or GND Im getting 4035 or 0 values
I checked ADC settings everything seems to be normal
I changed FW package version
static void MX_ADC_Init(void)
{
/* USER CODE BEGIN ADC_Init 0 */
/* USER CODE END ADC_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC_Init 1 */
/* USER CODE END ADC_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc.Instance = ADC1;
hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
hadc.Init.ContinuousConvMode = ENABLE;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC_Init 2 */
/* USER CODE END ADC_Init 2 */
}
Thanks,