2024-03-06 1:25 AM
Hi,
I want to update multiple HRTIM registers with a single DMA request on a STM32G474RE. To do this, I am trying to follow this simple Getting started with HRTIM tutorial, which has a section "#To_go_further_about_DMA_burst" on the board "B-G474E-DPOW1".
At the end of the tutorial we should see the CMP1xR updated with the value we set in Reg_Update after executing the HAL_HRTIM_BurstDMATransfer call in the debugger, but the register is not updated.
I followed the tutorial exactly, using CubeIDE to configure and generate code.
My analysis:
Going deeper into the function calls, I can see that the CPAR and CMAR registers are set correctly: CPAR contains the address of BDMADR (0x400177f0) and CMAR contains the address of Reg_Update (0x20000000). Then DMA is enabled and every statuses returned by HAL_DMA_Start_IT and HAL_HRTIM_BurstDMATransfer are HAL_OK. But there is no transfer to the CMP1xR.
My conclusions:
What I also tried:
Did I miss something? Do you have any idea why the CMP1xR is not updated?
2024-03-11 3:13 AM
Hello @PGONOVEA,
Thank you for your comment, which has helped us to improve the article !
Indeed, one step is missing. You need to declare the direction as being from memory to memory in the HRTIM DMA handler :
hdma_hrtim1_a.Init.Direction = DMA_MEMORY_TO_MEMORY;
Can you try and tell me if it's better now ?
Kind Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.