cancel
Showing results for 
Search instead for 
Did you mean: 

NO ST-Link Detected with MDK-ARM

rgalbany2
Associate II
Posted on March 23, 2011 at 08:14

Hello,

I'm totally novice and need your help.

I have installed the lastest version of the MDK-ARM from keil.

The result of the compilation is good, but when try to download the programm to the uC, the Software launch one message: ''

NO ST-Link Detected

''.

When I connect the DISCOVERY board to my USB, the led Blinks correctly, and 

and

I

could

update

the

firmware

of

the

system without

problems

.

Where is my problem?

Thanks!
12 REPLIES 12
rgalbany2
Associate II
Posted on March 31, 2011 at 22:14

I loaded one video in youtube with my problems:

http://www.youtube.com/watch?v=04arhw9JqWQ

rgalbany2
Associate II
Posted on April 05, 2011 at 08:25

Hi!

 

 

tested!! the Discovery board works fine with WinXP in english, but don't works if the language is in Spanish !!!!! Using Vista & Spanish language also don't woks!!

 

 

The past week I have sent one email to ST, but not have receiver any reply yet. Please correct this BUG Sirs of ST !!!

 

 

Regards,

 

 

Raul.
evgentusbachinintus
Associate II
Posted on July 27, 2012 at 02:57

I find a short video about this problem which advices some ways to solving this problem. I was approached last piece of advice

 Here is the Youtube Link  

http://www.youtube.com/watch?v=2mNc-v-OWSY&feature=plcp