2011-03-23 12:14 AM
Hello,
I'm totally novice and need your help. I have installed the lastest version of the MDK-ARM from keil. The result of the compilation is good, but when try to download the programm to the uC, the Software launch one message: ''NO ST-Link Detected
''. When I connect the DISCOVERY board to my USB, the led Blinks correctly, andand
I
could
update
the
firmware
of
the
system without
problems
.
Where is my problem? Thanks!2011-03-31 1:14 PM
2011-04-04 11:25 PM
tested!! the Discovery board works fine with WinXP in english, but don't works if the language is in Spanish !!!!! Using Vista & Spanish language also don't woks!!
The past week I have sent one email to ST, but not have receiver any reply yet. Please correct this BUG Sirs of ST !!!
Regards,
Raul.
2012-07-26 5:57 PM
I find a short video about this problem which advices some ways to solving this problem. I was approached last piece of advice
Here is the Youtube Link