cancel
Showing results for 
Search instead for 
Did you mean: 

Problem to connect the STM32F4DISCOVERY with ST-Link

jean_prieur
Associate III
Posted on March 24, 2012 at 11:21

Hello,

I just receive my STM32F4DISCOVERY. I installed IAR EWARM, and ST-Link driver V2. But after several tests on two laptops, I am unable to link the discovery board with ST-Link.

This is the message displayed: ''Fatal error - ST-Link connection error Session aborded!''

And this is the message on ST-Link utility: ''No ST-Link detected''

Do you have any idea of what happened? Thanks!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jean_prieur
Associate III
Posted on March 24, 2012 at 11:44

Ok I find the problem! IAR provided the ST-Link V2 driver, but it's not the latest version and it is not compactible with Windows Seven... Download ST-Link V2 driver on ST.com !

evgentusbachinintus
Associate II
Posted on July 27, 2012 at 03:02

I find a short video about this problem which advices some ways to solving this problem. I was approached last piece of advice

 Here is the Youtube Link 

http://www.youtube.com/watch?v=2mNc-v-OWSY&feature=plcp