cancel
Showing results for 
Search instead for 
Did you mean: 

''No STLink Detected''

muhammad
Associate II
Posted on June 27, 2012 at 15:11

hi all

i am using STM32F407VGT6 Discovery borad, with Keil MDK 4 compiler 

it was working perfectly, i just update the firmware and when i try to start debugging the updated firmware  Keil MDK shows the notification ''No STLink Detected'' and i am stucked just here. not getting any solution.

i had tried the STLink test, it works correctly but i get the mentioned error whenever i do try to start debugging..............

any help will be appreciated a looooot.....:)
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
frankmeyer9
Associate II
Posted on June 27, 2012 at 16:28

For unknown reasons, the stm32f0_discovery, which is supposedly newer than the stm32f4_discovery, works for me only when using the ''ST-Link (Deprecated Version)'' as debug adapter. I'm using Keil uVision V4.50 on WinXP in this case.

You could try that.

muhammad
Associate II
Posted on June 28, 2012 at 09:08

thanks for the assistance

actually my STLINK's version was incorrectly updated by Keil MDk 4.

now i just bust the older version into the STLINK. and its working perfect.

M2*

evgentusbachinintus
Associate II
Posted on July 27, 2012 at 02:53