cancel
Showing results for 
Search instead for 
Did you mean: 

No activity observed in Tx pin of FDCAN in STM32G491KCU6

ssuresh
Associate II

Hi STM Expert,

We are currently working on STM32G491KCU6 MCU FDCAN side. Our requirement is to validate the activity on Tx and Rx pins.

We started off the testing with the LoopBack mechanism but unfortunately we were not able to see any data received in the Rx buffer. We referred sample FDCAN programs for this and tested the same in STM IDE Debugger mode.

We then moved to test the normal mode as well. For this we used a sample code and probed the Tx pin of FDCAN using an oscilloscope. During the transmission, no activity is seen on the oscilloscope.

We confirmed the pins are not damaged by setting FDCAN_Tx and FDCAN_Rx pins to GPIO and toggled it.

 

Please let us know what we have missed and guide us.

28 REPLIES 28
ssuresh
Associate II

We face issues while opening the project.

Meanwhile can you let us know if you have modified anything on the code or ioc file shared to you by us?

Also, PB6 IO is made HIGH?

Hello,

I didn't remember that I modified something on the configuration. The are some screenshots of CubeMx:

SofLit_0-1729689117377.pngSofLit_1-1729689148420.png

SofLit_2-1729689191419.png

SofLit_3-1729689231590.png

At this stage I prefer that you share your schematics mainly the CAN part.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi Expert,

Please find the screenshots of CAN part schematics.

 

Hello,

I don't see any issue in the CAN HW.

Did you test the project I shared and probed CAN frame on PB6?

Is Rx interrupt firing?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi Expert,

We tried the same project you shared, but no change in the observation. No activity on Tx pin while probing.

Please look into screenshot below:

ssuresh_1-1729841748352.png

 

We are running the code in Debugger mode.

We can see that Tx buffer is getting filled up on executing the code and once Tx buffer is fully filled with 8 bytes, Rx buffer starts to get filled, but only 2 bytes.

Can you let us know if this is the expected behaviour? Why Rx buffer is not fully filled?

Is Rx interrupt firing? ---> How can we check this? Is there any register for this?


@ssuresh wrote:

No activity on Tx pin while probing.


Here I'm sure this is not a software issue. Please check again if you are probing on PB6. Check also if you set good parameter on the oscilloscope/Trigger to catch the frame.


@ssuresh wrote:

Hi Expert,

We tried the same project you shared, but no change in the observation. No activity on Tx pin while probing.

Please look into screenshot below:

ssuresh_1-1729841748352.png

 

We are running the code in Debugger mode.


Since you are receiving data, it's a good step.

 


@ssuresh wrote:

We can see that Tx buffer is getting filled up on executing the code and once Tx buffer is fully filled with 8 bytes, Rx buffer starts to get filled, but only 2 bytes.

Can you let us know if this is the expected behaviour? Why Rx buffer is not fully filled?

Is Rx interrupt firing? ---> How can we check this? Is there any register for this?


Simply because the Tx DLC = 2:

TxHeader.DataLength = FDCAN_DLC_BYTES_2;

Need to modify it to be:

TxHeader.DataLength = FDCAN_DLC_BYTES_8;

My question is: are you familiar with CAN? If not you need to get familiar with it in order to trouble shoot issues.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi Expert,

Modified the DataLength parameter to below one and now Rx buffer is getting filled. Thanks for the response.

TxHeader.DataLength = FDCAN_DLC_BYTES_8;

But still we could not observe activity on Tx pin in Debugger mode.

 

Then we disabled the debugger mode and simply booted our system. At this point, we were able to see continuous activity on Tx pin as below

ssuresh_0-1729856871288.jpeg

Cannot understand why it did not work when MCU was in debugger mode.

 

Now let us try the Normal mode and get back to you!

 

are you familiar with CAN? If not you need to get familiar with it in order to trouble shoot issues -->

No, CAN is new to me.

Hello,

Since the first issue has been solved : Frames are seen on Tx. We can close this thread.

Please open a new thread for this behavior on Debug mode.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

The new thread:

https://community.st.com/t5/stm32-mcus-products/fdcan-normal-mode-in-stm32g491kcu6/td-p/737208

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.