cancel
Showing results for 
Search instead for 
Did you mean: 

Multi Channel ADC with DMA on a NUCLEO H753ZIT6

LopsidedCoder
Associate II

I'm just getting started with STM32 microcontrollers and I have been using the NUCLEO H753ZIT6. I was trying to learn how to use multiple channels of ADC's with DMA. I was able to get some data when I used a single channel ADC normally. But now I'm not even able to get any data when I put the ADC data storing array in the "Live Expressions" tab. I have also tried to use timers to make the ADC conversions happen at a frequency of 10Hz. I have attached images of how I've setup the ADC and Timer. My timer configuration has a prescaler of 64000-1 because the Timer clock is running at 64 MHz. My ADC is running at a clock of 40 MHz because I thought if its less then it may work. I have also tried the "Continuous Conversion Mode" in the ADC setting and the "Circular mode" in the DMA setting but none of them work. This is my main.c file:

 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2025 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define ADC_BUFSIZE 20
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc3;
DMA_HandleTypeDef hdma_adc3;

TIM_HandleTypeDef htim2;

/* USER CODE BEGIN PV */
uint32_t ADC_BUFFER[ADC_BUFSIZE];
uint8_t adc_ready = 0;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_BDMA_Init(void);
static void MX_ADC3_Init(void);
static void MX_TIM2_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* Enable the CPU Cache */

  /* Enable I-Cache---------------------------------------------------------*/
  SCB_EnableICache();

  /* Enable D-Cache---------------------------------------------------------*/
  SCB_EnableDCache();

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_BDMA_Init();
  MX_ADC3_Init();
  MX_TIM2_Init();
  /* USER CODE BEGIN 2 */
  HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
  HAL_ADC_Start_DMA(&hadc3, ADC_BUFFER, ADC_BUFSIZE);
  HAL_TIM_Base_Start(&htim2);
  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {

  while(adc_ready != 1){

  }
  adc_ready = 0;
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Supply configuration update enable
  */
  HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

  /** Configure the main internal regulator output voltage
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

  /** Macro to configure the PLL clock source
  */
  __HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSI);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
                              |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief ADC3 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_ADC3_Init(void)
{

  /* USER CODE BEGIN ADC3_Init 0 */

  /* USER CODE END ADC3_Init 0 */

  ADC_ChannelConfTypeDef sConfig = {0};

  /* USER CODE BEGIN ADC3_Init 1 */

  /* USER CODE END ADC3_Init 1 */

  /** Common config
  */
  hadc3.Instance = ADC3;
  hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2;
  hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE;
  hadc3.Init.EOCSelection = ADC_EOC_SEQ_CONV;
  hadc3.Init.LowPowerAutoWait = DISABLE;
  hadc3.Init.ContinuousConvMode = ENABLE;
  hadc3.Init.NbrOfConversion = 2;
  hadc3.Init.DiscontinuousConvMode = DISABLE;
  hadc3.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
  hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
  hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
  hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
  hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
  hadc3.Init.OversamplingMode = DISABLE;
  hadc3.Init.Oversampling.Ratio = 1;
  if (HAL_ADC_Init(&hadc3) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
  sConfig.Channel = ADC_CHANNEL_5;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
  sConfig.SingleDiff = ADC_SINGLE_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;
  sConfig.OffsetSignedSaturation = DISABLE;
  if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
  sConfig.Channel = ADC_CHANNEL_4;
  sConfig.Rank = ADC_REGULAR_RANK_2;
  if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN ADC3_Init 2 */

  /* USER CODE END ADC3_Init 2 */

}

/**
  * @brief TIM2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_TIM2_Init(void)
{

  /* USER CODE BEGIN TIM2_Init 0 */

  /* USER CODE END TIM2_Init 0 */

  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};

  /* USER CODE BEGIN TIM2_Init 1 */

  /* USER CODE END TIM2_Init 1 */
  htim2.Instance = TIM2;
  htim2.Init.Prescaler = 16000-1;
  htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim2.Init.Period = 1000-1;
  htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM2_Init 2 */

  /* USER CODE END TIM2_Init 2 */

}

/**
  * Enable DMA controller clock
  */
static void MX_BDMA_Init(void)
{

  /* DMA controller clock enable */
  __HAL_RCC_BDMA_CLK_ENABLE();

  /* DMA interrupt init */
  /* BDMA_Channel0_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(BDMA_Channel0_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BDMA_Channel0_IRQn);

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOF_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOE_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOB, LD1_Pin|LD3_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pin : B1_Pin */
  GPIO_InitStruct.Pin = B1_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

  /*Configure GPIO pins : LD1_Pin LD3_Pin */
  GPIO_InitStruct.Pin = LD1_Pin|LD3_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  /*Configure GPIO pins : STLINK_RX_Pin STLINK_TX_Pin */
  GPIO_InitStruct.Pin = STLINK_RX_Pin|STLINK_TX_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

  /*Configure GPIO pin : LD2_Pin */
  GPIO_InitStruct.Pin = LD2_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
 /* Prevent unused argument(s) compilation warning */
 UNUSED(hadc);
 adc_ready = 1;
 HAL_ADC_Stop_DMA(&hadc3);

 /* NOTE : This function should not be modified. When the callback is needed,
           function HAL_ADC_ConvCpltCallback must be implemented in the user file.
  */
}
/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

1 ACCEPTED SOLUTION

Accepted Solutions

I see BDMA, seems like error.

Anyway, start from this example 

https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/ADC 

743 pretty much the same as 753.

View solution in original post

8 REPLIES 8
mƎALLEm
ST Employee

Hello @LopsidedCoder and welcome to the community,

Better to attach your ioc file instead of posting the screenshots of your configs and may be better to post a sketch of what do you want to achieve.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
TDK
Guru

Do the values show up in the array if you pause and examine with the Expressions tab?

Live Expressions is known to behave poorly.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for responding! I examined it with the Expressions tab and i got an Error: Target not available. I added a few breakpoints and it was normal till this line:

HAL_ADC_Start_DMA(&hadc3, ADC_BUFFER, ADC_BUFSIZE);

But when I went to the next breakpoint which was:

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
 /* Prevent unused argument(s) compilation warning */
 UNUSED(hadc);
 adc_ready = 1;
 HAL_ADC_Stop_DMA(&hadc3);

 /* NOTE : This function should not be modified. When the callback is needed,
           function HAL_ADC_ConvCpltCallback must be implemented in the user file.
  */
}

 it gave the target not found error.

I see BDMA, seems like error.

Anyway, start from this example 

https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/ADC 

743 pretty much the same as 753.

Hi, Thanks for the reply. I followed the Sample Code and it worked. I just had a small question, do we have to also include the configuration parameters like this:

  AdcHandle.Init.ClockPrescaler           = ADC_CLOCK_ASYNC_DIV2;            /* Asynchronous clock mode, input ADC clock divided by 2*/
  AdcHandle.Init.Resolution               = ADC_RESOLUTION_16B;              /* 16-bit resolution for converted data */
  AdcHandle.Init.ScanConvMode             = DISABLE;                         /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */
  AdcHandle.Init.EOCSelection             = ADC_EOC_SINGLE_CONV;             /* EOC flag picked-up to indicate conversion end */
  AdcHandle.Init.LowPowerAutoWait         = DISABLE;                         /* Auto-delayed conversion feature disabled */
  AdcHandle.Init.ContinuousConvMode       = ENABLE;                          /* Continuous mode enabled (automatic conversion restart after each conversion) */
  AdcHandle.Init.NbrOfConversion          = 1;                               /* Parameter discarded because sequencer is disabled */
  AdcHandle.Init.DiscontinuousConvMode    = DISABLE;                         /* Parameter discarded because sequencer is disabled */
  AdcHandle.Init.NbrOfDiscConversion      = 1;                               /* Parameter discarded because sequencer is disabled */
  AdcHandle.Init.ExternalTrigConv         = ADC_SOFTWARE_START;              /* Software start to trig the 1st conversion manually, without external event */
  AdcHandle.Init.ExternalTrigConvEdge     = ADC_EXTERNALTRIGCONVEDGE_NONE;   /* Parameter discarded because software trigger chosen */
  AdcHandle.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; /* ADC DMA circular requested */
  AdcHandle.Init.Overrun                  = ADC_OVR_DATA_OVERWRITTEN;        /* DR register is overwritten with the last conversion result in case of overrun */
  AdcHandle.Init.OversamplingMode         = DISABLE;                         /* No oversampling */

and this?

  /* ### - 3 - Channel configuration ######################################## */
  sConfig.Channel      = ADCx_CHANNEL;                /* Sampled channel number */
  sConfig.Rank         = ADC_REGULAR_RANK_1;          /* Rank of sampled channel number ADCx_CHANNEL */
  sConfig.SamplingTime = ADC_SAMPLETIME_810CYCLES_5;   /* Sampling time (number of clock cycles unit) */
  sConfig.SingleDiff   = ADC_SINGLE_ENDED;            /* Single-ended input channel */
  sConfig.OffsetNumber = ADC_OFFSET_NONE;             /* No offset subtraction */ 
  sConfig.Offset = 0;                                 /* Parameter discarded because offset correction is disabled */

I already do this setup in the IOC file's ADC parameters. Either way, I was able to get the readings in the Live Expressions tab for every 2 index of the array because I had only initialized two channels of ADC1(and one of the sensors weren't working, so i got a 0 reading from it), so im guessing the two sensors were filling up the array after each loop. I also did the sConfig configuration thing for both channels i just wanted to know if i need to do that or the setup i do in the IOC file is enough.


@MasterT wrote:

I see BDMA, seems like error.


Indeed.

@LopsidedCoder  see this article

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Understood, thanks a lot! I'm still a bit confused if I have to code the ADC configuration parameters or if its the same as doing it in the IOC file.


@LopsidedCoder wrote:
  AdcHandle.Init.ClockPrescaler           = ADC_CLOCK_ASYNC_DIV2;            /* Asynchronous clock mode, input ADC clock divided by 2*/
  AdcHandle.Init.Resolution               = ADC_RESOLUTION_16B;              /* 16-bit resolution for converted data */
  AdcHandle.Init.ScanConvMode             = DISABLE;                         /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */
  AdcHandle.Init.EOCSelection             = ADC_EOC_SINGLE_CONV;             /* EOC flag picked-up to indicate conversion end */
  AdcHandle.Init.LowPowerAutoWait         = DISABLE;                         /* Auto-delayed conversion feature disabled */
  AdcHandle.Init.ContinuousConvMode       = ENABLE;                          /* Continuous mode enabled (automatic conversion restart after each conversion) */
  AdcHandle.Init.NbrOfConversion          = 1;                               /* Parameter discarded because sequencer is disabled */
  AdcHandle.Init.DiscontinuousConvMode    = DISABLE;                         /* Parameter discarded because sequencer is disabled */
  AdcHandle.Init.NbrOfDiscConversion      = 1;                               /* Parameter discarded because sequencer is disabled */
  AdcHandle.Init.ExternalTrigConv         = ADC_SOFTWARE_START;              /* Software start to trig the 1st conversion manually, without external event */
  AdcHandle.Init.ExternalTrigConvEdge     = ADC_EXTERNALTRIGCONVEDGE_NONE;   /* Parameter discarded because software trigger chosen */
  AdcHandle.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; /* ADC DMA circular requested */
  AdcHandle.Init.Overrun                  = ADC_OVR_DATA_OVERWRITTEN;        /* DR register is overwritten with the last conversion result in case of overrun */
  AdcHandle.Init.OversamplingMode         = DISABLE;                         /* No oversampling */

and this?

  /* ### - 3 - Channel configuration ######################################## */
  sConfig.Channel      = ADCx_CHANNEL;                /* Sampled channel number */
  sConfig.Rank         = ADC_REGULAR_RANK_1;          /* Rank of sampled channel number ADCx_CHANNEL */
  sConfig.SamplingTime = ADC_SAMPLETIME_810CYCLES_5;   /* Sampling time (number of clock cycles unit) */
  sConfig.SingleDiff   = ADC_SINGLE_ENDED;            /* Single-ended input channel */
  sConfig.OffsetNumber = ADC_OFFSET_NONE;             /* No offset subtraction */ 
  sConfig.Offset = 0;                                 /* Parameter discarded because offset correction is disabled */

 


You can configure and generate that code with CubeMx.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.