cancel
Showing results for 
Search instead for 
Did you mean: 

Mistake in STM32G4xx Reference Manual (RM0440)?

TwelveSquared
Senior

The STM32G4xx Reference Manual (RM0440) Rev 4, Figure 2, "Memory Map" on Page 81 says Option Bytes 1 is from 0x1fff7800 to 0x1fff7810 (16 option bytes), Option Bytes 2 is from 0x1ffff800 to 0x1ffff810 (16 option bytes).

However:

Table 7 on page 94 says: Option Bytes 1 is from 0x1fff7800 to 0x1fff782f (48 option bytes) and Option Bytes 2 is from 0x1ffff800 to 0x1ffff82f (48 option bytes).

Is this discrepancy an error?

If not an error, please help me understand!!

Thanks kindly,

2 REPLIES 2
Imen.D
ST Employee

Hello @TwelveSquared​ ,

You are right. I raised your feedback internally to correct adresses in the Figure 2 "Memory Map" in RM0440:

So, 0x1FFF 7810 and 0x1FFF F810 will be updated to 0x1FFF 7830 and 0x1FFF F830.

Thank you for your contribution.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Hello @Imen DAHMEN​ 

Thank you for confirming and raising the issue internally. Looking forward to the corrected datasheet.

Thanks