cancel
Showing results for 
Search instead for 
Did you mean: 

Missing USB CDC NUCLEO-F746ZG Cube Sample

Adam Davis
Associate II

Hello all.

I'm trying to find a CDC same for the NUCLEO-F746ZG board but the latest cube I've downloaded (STM32Cube_FW_F7_V1.12.0) only contains the following:

  • DFU_Standalone
  • HID_Standalone
  • MSC_Standalone

Could somebody please point me where I could find an example of setting up CDC for the NUCLEO-F746ZG board please?

Thanks

1 REPLY 1
Imen.D
ST Employee

Hello,

There is no CDC example for the NUCLEO-F746ZG board available with STM32CubeF7 firmware package. But, there are CDC examples with STM32756G-EVAL and STM32F769I-EVAL. So, you can get inspired from one of these applications to develop your application.

Note that the available HAL examples are listed in this application note AN4731 : "STM32Cube firmware examples" .

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen