2024-10-21 12:03 AM
Hi I am using below controller in one of our design
STM32G474CET3
i would like to know minimum external clock frequency on which my microcontroller works.
Also my requirement includes 1 SPI, 1 I2C and 4 ADC input sensing.
I would need very minimum external clock frequency on which it can ru,
And ultimate goal is to run 1 SPI, 1 I2C and 4 ADC input sensing at a very low current consumption for 3.3V microcontroller supply,
In datasheet its mentioned from 4 MHz, can this be used in 1 to 3 MHz range too
Also any ball park current consumption can i get for 1 SPI, 1 I2C and 4 ADC input sensing at 3.3V input to Microcontroller.
Solved! Go to Solution.
2024-10-23 03:35 AM
For external clock, not external crystal, there is no lower limit.
2024-10-24 07:09 AM
Yes you are correct its not just a crystal
i am connecting external clock generation IC which generates 1 MHz clock,