cancel
Showing results for 
Search instead for 
Did you mean: 

Minimum external clock requirement for STM32G474CET3

sag
Associate III

Hi I am using below controller in one of our design

STM32G474CET3

 

i would like to know minimum external clock frequency on which my microcontroller works.

 

Also my requirement includes 1 SPI, 1 I2C and 4 ADC input sensing.

 

I would need very minimum external clock frequency on which it can ru,

And ultimate goal is to run 1 SPI, 1 I2C and 4 ADC input sensing at a very low current consumption for 3.3V microcontroller supply,

 

In datasheet its mentioned from 4 MHz, can this be used in 1 to 3 MHz range too

sag_0-1729494067687.png

Also any ball park current consumption can i get for 1 SPI, 1 I2C and 4 ADC input sensing at 3.3V input to Microcontroller.

 

11 REPLIES 11
Uwe Bonnes
Principal III

For external clock, not external crystal, there is no lower limit.

Yes you are correct its not just a crystal

i am connecting external clock generation IC which generates 1 MHz clock,