cancel
Showing results for 
Search instead for 
Did you mean: 

MB1549-U575ZIQ-C03 Board ,FDCAN don't work at FDCAN_MODE_NORMAL

dylanou
Associate III

board:MB1549-U575ZIQ-C03  (mcu stm32U575)

I debug the FDCNA function with a CANalyst tool 

1. Work at FDCAN_MODE_BUS_MONITORING mode, It can receive data from the CANalyst tool 

2. Work at FDCAN_MODE_EXTERNAL_LOOPBACK,It can receive data itself and the canslyst tool can receive the data

3. Work at FDCAN_MODE_NORMAL, It cann't receive data,and send data fail 

void MX_FDCAN1_Init(void)

{

hfdcan1.Instance = FDCAN1;

hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;

hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;

hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;

hfdcan1.Init.AutoRetransmission = DISABLE;

hfdcan1.Init.TransmitPause = DISABLE;

hfdcan1.Init.ProtocolException = DISABLE;

hfdcan1.Init.NominalPrescaler = 32;

hfdcan1.Init.NominalSyncJumpWidth = 1;

hfdcan1.Init.NominalTimeSeg1 = 2;

hfdcan1.Init.NominalTimeSeg2 = 2;

hfdcan1.Init.DataPrescaler = 1;

hfdcan1.Init.DataSyncJumpWidth = 1;

hfdcan1.Init.DataTimeSeg1 = 1;

hfdcan1.Init.DataTimeSeg2 = 1;

hfdcan1.Init.StdFiltersNbr = 0;

hfdcan1.Init.ExtFiltersNbr = 0;

hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_QUEUE_OPERATION;

if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)

{

Error_Handler();

}

#if 1

FDCAN_FilterTypeDef FDCAN1_RXFilter;

FDCAN1_RXFilter.IdType=FDCAN_STANDARD_ID;

FDCAN1_RXFilter.FilterIndex=0;

FDCAN1_RXFilter.FilterType=FDCAN_FILTER_RANGE;

FDCAN1_RXFilter.FilterConfig=FDCAN_FILTER_TO_RXFIFO0;

FDCAN1_RXFilter.FilterID1=0x0000;

FDCAN1_RXFilter.FilterID2=0x0000;

if(HAL_FDCAN_ConfigFilter(&hfdcan1,&FDCAN1_RXFilter)!=HAL_OK)

{

Error_Handler();

}





HAL_FDCAN_Start(&hfdcan1);

HAL_FDCAN_ActivateNotification(&hfdcan1,FDCAN_IT_RX_FIFO0_NEW_MESSAGE,0);

#endif



/* USER CODE END FDCAN1_Init 2 */



}



void HAL_FDCAN_MspInit(FDCAN_HandleTypeDef* fdcanHandle)

{



GPIO_InitTypeDef GPIO_InitStruct = {0};

RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

if(fdcanHandle->Instance==FDCAN1)

{

/* USER CODE BEGIN FDCAN1_MspInit 0 */



/* USER CODE END FDCAN1_MspInit 0 */



/** Initializes the peripherals clock

*/

PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_FDCAN1;

PeriphClkInit.Fdcan1ClockSelection = RCC_FDCAN1CLKSOURCE_PLL1;

if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

{

Error_Handler();

}

/* FDCAN1 clock enable */

__HAL_RCC_FDCAN1_CLK_ENABLE();



__HAL_RCC_GPIOD_CLK_ENABLE();

/**FDCAN1 GPIO Configuration

PD0 ------> FDCAN1_RX

PD1 ------> FDCAN1_TX

*/

GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_PULLUP;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;

HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);



/* FDCAN1 interrupt Init */

HAL_NVIC_SetPriority(FDCAN1_IT0_IRQn, 4, 0);

HAL_NVIC_EnableIRQ(FDCAN1_IT0_IRQn);

/* USER CODE BEGIN FDCAN1_MspInit 1 */



/* USER CODE END FDCAN1_MspInit 1 */

}

}

uint8_t FDCAN1_Send_Msg(uint8_t* msg)

{



fdcan1_TxHeader.Identifier = 0x001;

fdcan1_TxHeader.IdType = FDCAN_STANDARD_ID;

fdcan1_TxHeader.TxFrameType = FDCAN_DATA_FRAME;

fdcan1_TxHeader.DataLength = FDCAN_DLC_BYTES_8;

fdcan1_TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;

fdcan1_TxHeader.BitRateSwitch = FDCAN_BRS_OFF;

fdcan1_TxHeader.FDFormat = FDCAN_CLASSIC_CAN;

fdcan1_TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;

fdcan1_TxHeader.MessageMarker = 0x52;



if(HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1,&fdcan1_TxHeader,msg)!=HAL_OK) return 1;//发送

return 0;

}

void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)

{

/* Prevent unused argument(s) compilation warning */

UNUSED(hfdcan);

UNUSED(RxFifo0ITs);



if((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != RESET)

{

/* Retrieve Rx messages from RX FIFO0 */

memset(RxData, 0, sizeof(RxData));

if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)

{

Error_Handler();

}
}
}

 

1 ACCEPTED SOLUTION

Accepted Solutions
dylanou
Associate III

Thand you for your reply

I find the cause of the problem

The transceiver need to power of 5V, but I only provide 3.3V

View solution in original post

8 REPLIES 8
dylanou
Associate III

 

hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;   // can not work

 

hfdcan1.Init.Mode = FDCAN_MODE_BUS_MONITORING;   //  work well

 

hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK;   //  work well

 

Hello,

  1. Are you using a transceiver with another CAN node connected to the bus?  if it's not the case it won't work.
  2. These values are not recommended for CAN bit time settings::
    hfdcan1.Init.NominalPrescaler = 32;
    hfdcan1.Init.NominalTimeSeg1 = 2;
    hfdcan1.Init.NominalTimeSeg2 = 2

    See my answer in this thread.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
dylanou
Associate III

Are you using a transceiver with another CAN node connected to the bus?

1. had can  transceiver

dylanou_0-1713402314461.png

 

dylanou
Associate III

work at FDCAN_MODE_BUS_MONITORING or  FDCAN_MODE_EXTERNAL_LOOPBACK ,It can receive or send data

dylanou
Associate III
 
 

config.png

dylanou
Associate III

I change below,but it doesn't work too

hfdcan1.Instance = FDCAN1;

hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV10;

hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;

hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;

hfdcan1.Init.AutoRetransmission = DISABLE;

hfdcan1.Init.TransmitPause = DISABLE;

hfdcan1.Init.ProtocolException = DISABLE;

hfdcan1.Init.NominalPrescaler = 2;

hfdcan1.Init.NominalSyncJumpWidth = 1;

hfdcan1.Init.NominalTimeSeg1 = 12;

hfdcan1.Init.NominalTimeSeg2 = 3;

hfdcan1.Init.DataPrescaler = 1;

hfdcan1.Init.DataSyncJumpWidth = 1;

hfdcan1.Init.DataTimeSeg1 = 1;

hfdcan1.Init.DataTimeSeg2 = 1;

hfdcan1.Init.StdFiltersNbr = 0;

hfdcan1.Init.ExtFiltersNbr = 0;

Hello,

  1. had can transceiver -> Need to provide more details about your transceiver's module: the transceiver datasheet + module schematics as this is an important point for analysis.
  2. work at FDCAN_MODE_BUS_MONITORING or FDCAN_MODE_EXTERNAL_LOOPBACK ,It can receive or send data. -> Expected behavior if there is a HW issue (external from the MCU: wiring, transceiver issue, clock source, not the correct CAN pins assigned etc ..) the CAN won't work. Loopback and Monitoring are less restrictive.
  3. Need to monitor CAN_Rx (Not CAN_H nor CAN_L) with an oscilloscope or logic analyzer. Do you see CAN activity on CAN_Rx?
  4. You need also to share your project (at least the ioc file)

PS: please use </> button to insert your code.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
dylanou
Associate III

Thand you for your reply

I find the cause of the problem

The transceiver need to power of 5V, but I only provide 3.3V