cancel
Showing results for 
Search instead for 
Did you mean: 

Multi ADC in parallel

giwonKIM
Associate III

Hi, I'm using  multi channels ADC3 of "STM32H735ZGT6" (3channels)

 

I want to use these channels in parallel, but I've only found a way to convert in order in the Datasheet.

Can I run all the ADC3's channels at once in parallel?

If that is the case, can I get a reference manual or some advice?

If you want to see my CUBEMX or Code, Please tell me.

 

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
GwenoleB
ST Employee

Hello @giwonKIM,

ADC3 (in addition ADC1/2) does not allow parallel conversion. 
You can only configure a sequence of channel rank to chain them. Or, if you absolutely need to convert them in parallel, use 1 ADC per channel.

I hope it answers to your question.

Kind regards,

Gwénolé

 

View solution in original post

2 REPLIES 2
GwenoleB
ST Employee

Hello @giwonKIM,

ADC3 (in addition ADC1/2) does not allow parallel conversion. 
You can only configure a sequence of channel rank to chain them. Or, if you absolutely need to convert them in parallel, use 1 ADC per channel.

I hope it answers to your question.

Kind regards,

Gwénolé

 

giwonKIM
Associate III

giwonKIM_0-1713486800514.png

I organized 3 channels of ADC3 like this picture.

As you said, do you mean you can't convert 3 channels (IN0,IN1,IN10) at the same time and can do it in order?

 

If so, should we use each channel of 3 ADC blocks (ADC1, ADC2, ADC3) as shown in the picture below to convert at the same time?

화면 캡처 2024-04-19 094322.png

giwonKIM_2-1713487441327.png