2024-11-28 7:30 AM
Hi,
I'm using STM32H745ZI implemented ethernet with Lwip it's working fine STM32CubeIDE(ver-1.90.0) but not in IAR(ver-9.30.1) like any changes that I need to do in .icf file of IAR because it's working fine Cube IDE
2024-11-28 7:51 AM
Have you tried debugging in IAR to what's failing, and where?
Do you have any other project(s) that work(s) on both STM32CubeIDE and IAR ?
2024-11-28 8:02 AM
ping(IP address) is not working in IAR (request message come back in command cmd), Actually the same project is working in both IAR and CubeIDE but when I added Ethernet Lwip it stopped working in IAR
2024-11-28 8:44 AM
Enable LwIP diagnostic traces in both.
Compare & contrast ...
2024-11-28 9:00 AM
How to do that?
2024-11-28 9:08 AM
2024-11-28 12:05 PM
Dear @Lucifer37 ,
in same cases, it is a matter to increase inside the .icf file the heap and stack size for RAM areas , check both linkers file and try to increase to a larger allocation .
Hope it helps ,
STOne-32
2024-12-06 10:46 PM
Hi @STOne-32 , @Andrew Neil
When FDCAN is enable it receiving data through CAN bus at that time Ethernet is not working, In middle some times response ping is working, After resetting stm32 board ping is working but after some times it stopped working,
Does FDCAN cause problem, because FDCAN receiving more data like more traffic is there so ethernet timeout happening. FDCAN using at 500kbps
After removing FDCAN it's working perfectly fine..............WHY I want both should work FINE...