2023-04-03 1:32 PM
I'm having a significant problem debugging my board with CAN traffic. Whenever the debugger is paused, and a CAN message is received via interrupt, the independent watchdog is being reset. As far as I can tell, I'm disabling that peripheral on debug correctly, but anytime I set a breakpoint, the IWDG is resetting the MCU. If my board does NOT receive any CAN messages, everything works as expected.
Relevant Information
Below is my code for disabling peripherals for debugging:
//Halt Interrupts on Debug stop
__HAL_RCC_DBGMCU_CLK_ENABLE();
__HAL_FREEZE_IWDG_DBGMCU();
__HAL_FREEZE_WWDG_DBGMCU();
__HAL_FREEZE_TIM1_DBGMCU();
__HAL_FREEZE_TIM2_DBGMCU();
__HAL_FREEZE_TIM3_DBGMCU();
__HAL_FREEZE_TIM16_DBGMCU();
__HAL_FREEZE_CAN_DBGMCU();
Disabling the watchdog entirely appeared to work, but pausing in the debugger only allows me to debug the CAN interrupt, so it seems when the debugger is paused, the MCU gets stuck in the CAN interrupt.
Solved! Go to Solution.
2023-05-05 6:37 AM
So, I actually did manage to solve the problem.
I was reorganizing my code, and choosing a different implementation for initializing CAN hardware. The new implementation removed these three lines:
RCC->APB1RSTR &= ~RCC_APB1RSTR_CANRST;
RCC->APB1ENR |= RCC_APB1ENR_CANEN;
CAN->MCR = 0x00008000;
After that, I was able to debug as normal. Not exactly sure which line is the culprit but... problem solved...
2023-05-05 2:33 AM
Hello @sonic1015, and welcome to ST Community,
As far as you explained, I think it's a timing issue
>> The MCU gets stuck in the CAN interrupt
I also think that when the debugger is paused, the CAN message interrupts the MCU, which causes the watchdog to reset since the interrupt takes too long to process...
You can try to increase the CAN interrupt priority so that it will be processed first and the watchdog won't reset the MCU!
I hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-05 6:37 AM
So, I actually did manage to solve the problem.
I was reorganizing my code, and choosing a different implementation for initializing CAN hardware. The new implementation removed these three lines:
RCC->APB1RSTR &= ~RCC_APB1RSTR_CANRST;
RCC->APB1ENR |= RCC_APB1ENR_CANEN;
CAN->MCR = 0x00008000;
After that, I was able to debug as normal. Not exactly sure which line is the culprit but... problem solved...