cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with receiving FDCAN data with STM3232H750

revvathi
Associate II

I have debugged the whole code to send data from stm32h750b-dk between the two fdcan terminals fdcan1 and fdcan2 the data is appearing on live expressions of txdata1 but in rxdata only 1 bit is being transferred can somebody mention what the problem could be 
all my parameters are adjusted accurately 

Txdata[2]={7,8};

this is the output which is shown can somebody help me out on wtt could be done

kl.png

10 REPLIES 10

thank u so much it worked after fitting jumpers on jp6 and jp7

<3