STM32G474 FDCAN Interrupt does not trigger
- December 4, 2024
- 1 reply
- 681 views
The FDCAN (in my case fdcan2) for a custom board based on STM32G474RCT that I am working on does not seem to work as expected. The transmission of messages is working OK. I can receive the test message from the board over to the host PC CAN sniffer at 250K baud. I have tried to use the example project for the Classic CAN Networking using FDCAN.
So though transmission is working, reception requires an interrupt which never comes. I have traces from the oscilloscope that confirm the GPIO pin responsible for FDCAN2 Rx is receiving signal from the on board CAN Transceiver, but the controller does not respond reception with the interrupt call.
I have attached the bare minimum example as a STM32CubeIDE project to help find a solution in my situation.
Thanks for having a look.
Cheers