2024-07-15 12:44 AM
Hello all,
We are evaluate STM32H745 for one of our new products. Dual core feature of STM32H745 is something we would like to use.
As a part of initial process, I was trying to debug both M4 and M7 cores simultaneusly.
Following AN5286, I was able to succesfully debug both core using STM32Cube IDE.
But when I tried following in section 4, to use IAR workbench I got following error
What I have found is ticking multicore support in IAR gives the erro
I was able to debug individual cores if I don't enable multicore.
Any guidance is deeply appreciated.
2024-07-15 02:12 AM
Hello,
Refer to the AN5286 "STM32H7x5/x7 dual-core microcontroller debugging", section 4 Using IAR Embedded Workbench™ for Arm®
2024-07-15 02:26 AM
Make sure IAR version you're using has most current drivers and DLLs for ST-LINK installed.
Check for IAR IDE patches in CubeH7 Software directory in repo or ZIP file.
2024-07-15 02:48 AM
Many thanks for the quick response.
@SofLitAs mentioned in my original post, I have already followed AN5286.
@Tesla DeLoreanI copied all the patch files over to IAR "C:\Program Files\IAR Systems\Embedded Workbench 9.2\arm" and restarted IAR. But still getting the same error message.
2024-07-15 02:50 AM
The link you shared pointed to: https://www.st.com/resource/en/application_note/dm00629855-getting-started-with-projects-based-on-dualcore-stm32h7-microcontrollers-in-stm32cubeide-stmicroelectronics.pdf
Which is not the correct link
2024-07-15 02:52 AM
Appolgies for the wrong link. I have followed the AN5286 and landed to this issue.