2020-01-29 1:11 PM
2020-01-29 1:44 PM
I doubt this design is going to be revisited. Talk to local sales staff/engineers.
Review new parts for commonality of foot-print, 144-pin devices have generally had the best migration path.
2020-01-29 1:46 PM
STM32G474 has no ethernet but CANFD. Did you look at the new STM32H7 variant?
2020-01-29 1:59 PM
Yes, but, STM32H7 is too overloaded with features I dont need.
2020-01-29 2:12 PM
Generally I need Cortex-M4, >120Mhz, USB FS, CAN-FD (at least 2), and Ethernet MAC. STM32F407 is closest. I see all new MCUs (G0/G4/L5 lines) now utilize CAN-FD instead of old CAN, but have no Ethernet. So I expect some new chip like STM32F407 with CAN-FD. Microchip already has SAME54 - this one is exacly what I am looking for. But SAME54 has lots of drawbacks on overall design of the other chip peripherals (DMA, clocks, timers, ADC etc...)
2020-01-29 7:19 PM
So the STM32H7 has everything you need but you don't want to use it because it's "overloaded with features"? How is that a problem? Why not use what you want and leave the other features untouched?
2020-01-29 7:29 PM
The problem is its price
2020-01-29 7:58 PM
On Digikey (qty 1):
STM32F407 is $9.29
STM32H745 is $11.71
I doubt they're going to introduce a new line of chips between those two price points.
2020-01-29 8:36 PM
On our local distributor
STM32F407ZGT6 is about 5$
STM32H745 11$
2020-01-30 12:26 AM
Given the cost of all the other bits in a project (including the major one of time and effort writing and debugging the code), that sort of price-difference is negligible for small production runs (say 10 units).
And for larger production runs I'm sure you'll be able to get a better price. I've even known cases where the the price difference reverses in sufficient quantity.
Having said that, I've been trying to port some code from stm32f7 to stm32h7 for a long time and I'm still hitting differences.
Regards,
Danish