2021-02-13 1:45 AM
I've gone through AN2594 and the associated examples. They're all for the standard peripheral library which is now deprecated.
Someone has an example of a port on github that looks reasonably complete https://github.com/lamik/EEPROM-emulation-STM32F1-HAL/blob/master/Src/eeprom.c
and at this stage it looks like I will be using that
however...
I'm wondering it ST have (or are planning to have) an official update?
Solved! Go to Solution.
2021-02-13 1:51 AM
I thought they did, or had Cube auto-generate the boiler plate code.
2021-02-13 1:51 AM
I thought they did, or had Cube auto-generate the boiler plate code.
2021-02-13 1:26 PM
Thanks. Your suggestion regarding Cube generating the code sent me looking there.
I found that they ship examples in the CubeMX firmwares i.e. STM32Cube_FW_F1_V1.8.3
For the F4 firmware (STM32Cube_FW_F4_V1.25.2 ) the examples are selectable in the CubeMX example selector but not for the F1 examples.
:thumbs_up: