2023-02-22 12:08 PM
2023-02-22 12:49 PM
>>Those parts that had short lead times suddenly changed to more than a year out with no explanation.
Everyone ran to that side of the ship...
The fab is capacity bound, as more orders are placed, the availability pushes out. Demand for any part is high.
Moral here is to order the parts you want to receive, otherwise someone else will get them.
2023-03-08 09:37 AM
This forum thread was marked by the moderator as needing a little more investigation, so a Support case was created in your name and will be handled off-line. Should anyone have any similar questions, please feel free to open a Support case directly at your myST portal: https://st.com/ols
2023-03-08 11:00 PM
That's kinda funny answer...
So it is questioned if the "STM32H7 series parts" are still "made", and a support case is needed for that?
Everyone knows that demand is much higher than availability, so a better answer would be:
"Hell yeah, we see that the market needs more H7, so let's crank up production volume!"
;-)