Is it possible to change GPIO_Mode and GPIO PU/PD settings from Device configuration tool on STM32G0?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-09-08 8:50 AM
When I assign a pin to a peripheral (e.g. comparator 3) the corresponding GPIO mode is fixed to Analog and cannot be changed. As a consequence, no pull-up or pull-down resistor can be inserted. By changing System.ioc with a text editor the correct code is generated and the device behaves as expected (pull-up register inserted)
PE7.GPIOParameters=GPIO_Label
changed to
PE7.GPIOParameters=GPIO_PuPd,GPIO_Label,GPIO_Mode
Added rows:
PE7.GPIO_Mode=GPIO_MODE_AF_OD
PE7.GPIO_PuPd=GPIO_PULLUP
- Labels:
-
Bug-report
-
GPIO-EXTI
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-10-31 5:54 AM
The easier way to set pull-up or pull-down GPIO resistor is through direct register control in code:
GPIOE->PUPDR = (0x1 << (0x2U * 0x7));
where GPIOE is used GPIO port
0x1 is for pull-up resistor (0x0 - no pull-up no pull-down, 0x2 pull-down)
0x7 is the number of GPIO pin
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.