cancel
Showing results for 
Search instead for 
Did you mean: 

Input Capture Mode- STM32 MAT Target

Samuel1
Associate III

Hello everybody,

I want to measure   the duty Cycle of a PWM Signal in Simulink. . I have managed it to  generate a  PWM signal with Simulink and STM32 MAT-Target. The problem is  now when build  a simple model to generate the code, the lines between the blocks will turn  to red. and  thus  i am not  able to measure the duty cycle with input capture direct mode. Can someone help with this?

BR

#Pwm-input-capture​ #Simulink​ #PWM​ #[STM32-Mat/Target]​ #Matlab​ #TIMER​ #

0 REPLIES 0