cancel
Showing results for 
Search instead for 
Did you mean: 

Identifying Silicon Revision of STM32H735IGK6U

rk_iot
Associate II

Hello,

we are using STM32H735G-DK Eval Boards equipped with differently marked STM32H735IGK6U chips.

One saying:

-------------------

STM32H735

IGK6U

AA126   VQ Z

TWN AA 109

                    D2

--------------------

and the other one saying:

-------------------

STM32H735

IGK6U

AA126   VQ Z

TWN AA 109

                    D3

--------------------

We could not find the meaning of "D2" and "D3" but "D2" is producing HardFaults whereas "D3" is not so we are assuming that these do have different silicon revisions.

 

Could you help us identifying the silicon revision of the chips or what else is "D2" and "D3" standing for?

 

We also attached photos of the different markings.

 

Thank you and best regards

RK_IOT

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

The two chips having the same revision rev Z (the latest silicon revision).

You need to contact your local sales for D2 and D3 marking.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

2 REPLIES 2
SofLit
ST Employee

Hello,

The two chips having the same revision rev Z (the latest silicon revision).

You need to contact your local sales for D2 and D3 marking.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Both Z step, you can check via DEVID register. 

I think D2/D3 relates to line at plant.

Doubt this is cause of Hard Fault, dig deeper as to WHY it faults.

Likely clocks, power or flash wait states.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..