cancel
Showing results for 
Search instead for 
Did you mean: 

I2S STM32 Sampling frequency different from what reference manual states, why?

CLeo.1
Senior II

Hi Guys, in the reference sheet of the STM32H753ZI Pg. 2212 it says

"FWS is the audio sampling

frequency."

There's a programing example provided at Pg. 2232 that says Sampling Freq = 48kHz.

I tried this exact configuration, the MCLK, FWS, and SCLK are all correct, however when I see the sampling frequency its double of the FW?

The green signal is the On and Off when the DMA triggers. Sample buffer is length of 4

so it will trigger at 2 and 4. High is Complete and Low is Half Complete

Yellow signal is the FWS

0693W000004JWv8QAG.png 

CODE: MAIN()

uint16_t RxBuff[4];
uint16_t TxBuff[4];
uint8_t TC_Callback = 0;
uint8_t HC_Callback = 0;
char uartBuff[8];
void DMA1_Stream0_IRQHandler(void) {
	if (((DMA1 -> LISR) & (DMA_LISR_TCIF0)) != 0){
		DMA1 -> LIFCR |= DMA_LIFCR_CTCIF0;
		TC_Callback = 1;
	}
	else if (((DMA1 -> LISR) & (DMA_LISR_HTIF0)) != 0){
		 DMA1 -> LIFCR |= DMA_LIFCR_CHTIF0;
		 HC_Callback = 1;
	}
 
}
 
int main(void) {
	init_Clock();
	init_I2S();
	init_Debugging();
	init_Interrupt();
	init_SpeedTest();
  while (1)
  {
 
 
 
	  if (HC_Callback == 1){
		  GPIOA->BSRR |= GPIO_BSRR_BS3_HIGH;
		  HC_Callback = 0;
	  } else  if (TC_Callback == 1){
 
		  GPIOA->BSRR |= GPIO_BSRR_BR3_LOW;
		  TC_Callback = 0;
	  }
 
 
  }
}

 The math to find out the F_sample (Green Signal)

 Half Complete triggers every 20.6uS for every 2 Samples.

Thus in 1 second 97kSamples are obtained, which is close to 96kSamples and not 48kSamples as it was suggested from the reference manual

UPDATE 1:

I have tried making FWS = 96kHz this caused the sampling frequency to be closed to 192khz so it looks like the sampling frequency for I2S is FWS*2?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

I2S is inherently stereo, so you have 2 data per sample.

JW

View solution in original post

6 REPLIES 6
waclawek.jan
Super User

I2S is inherently stereo, so you have 2 data per sample.

JW

Ahhh, I was under the assumption since I made changes to the "FTHLV" register to be 1 data. So It would only transfer the Left side audio

waclawek.jan
Super User

I don't use the 'H7 and the SPI/I2S module there is a beast, but, AFAIK, FTHLV impacts only the "inward" SPI/I2S-to-processor interface, not the "outward" behaviour of the "protocol interface".

JW

Ahh thank you. I was curious if you could help me out on another question I posted here, Its about the Digital filter implementation via matlab to STM32H7

waclawek.jan
Super User

Sorry, I am neither into Matlab nor 'H7.

JW

CLeo.1
Senior II

Its fine, I figured it out I was at the wrong sampling rate. So The new issue is that I am making my FWS back to 48kHz now the I2S peripherals doesn't want to send data to the MCU but if I use FWS = 96kHz it works perfect? Any thoughts?