2025-05-18 1:42 AM
Hey, I just want to report an error in the Reference Manual for the STM32F411xC/E microcontroller.
Reference Manual: https://www.st.com/resource/en/reference_manual/rm0383-stm32f411xce-advanced-armbased-32bit-mcus-stmicroelectronics.pdf
Published on: https://www.st.com/en/microcontrollers-microprocessors/stm32f411/documentation.html
Error Description:
The error is in "Table 26. GPIO register map and reset values" on page 163. I recognized that the bit representation of the "Reset value" of the GPIOA_MODER register (the first one in Table 26) doesn't match with the value written on page 157.
I think it got copied from the Chinese version of the Reference Manual and only got changed on page 157, which I think is the right reset value. (It matches with the reset value in the SVD-file.)
Reset values:
page 157: 0xA800 0000
page 163: 0b0000 1100 0000 0000 0000 0000 0000 0000
Hopefully I'm not mistaken with this report.
All the best, wolkns.
2025-05-18 5:15 AM - edited 2025-05-25 11:51 PM
Hello @wolkns and welcome to the ST Community.
Thank you so much for reporting this typo. I've escalated this internally for correction on the future releases of the doc (under internal ticket number 210733).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.