2025-01-21 11:32 PM
Hello, this is DK.
I am working on a project using stm32f429IIt6.
I'm currently having an I2C problem at the end of my project.
I2C1 uses PF 0, 1 / I2C2 uses PB 6, 7. The HW PCB completed, and the HW I2C pull up is the same.
In I2C1 HAL code, the entire initialization does not work, and if I2C2 is used with the same code, it works well.
I am using various Pheripherals such as TIM Interrupt. Is there any conflict?
Is there any difference between I2C1 and I2C2?
In the TIMER part, it appears to share APB1.
2025-01-23 10:05 AM - edited 2025-01-23 10:06 AM
@Jdogk wrote:What means typo?
Misprint, typographical error. You wrote I2C3 here but talk about I2C1 issues.
2025-01-23 10:17 AM - edited 2025-01-23 10:20 AM
@Jdogk everyone can see all posts - there's no need to repeat posts with the same information.
You can mention several people in one post with @
2025-01-23 04:28 PM
I also use I2C3 in another IC(gyro sensor).
Error in I2C1
2025-01-23 04:31 PM
But your original question is just about I2C1 & I2C2.
Are you saying you also get problems with I2C3 in conjunction with I2C1 and/or I2C2?
Does each one work separately on its own?