cancel
Showing results for 
Search instead for 
Did you mean: 

I2C clock not working

Tendo
Associate II

Hi everybody !! i have an issue on I2C with a STM32 issue. i thought this was a code issue but in the main i also make LEDs blinking and it works, only the I2C doesn't work but... i noticed that my lines both rise to 3.3V but never fall down it just stay high. i guess it might be because i have a clock issue. Im using internal clock for some reasons, no external crystal. The HAL-delay function work with the SYSCLK but my I2C clock doesn't. Thx for your future answers. Best regards.

22 REPLIES 22

i tried to leave all my function and only put one I2C function in the main like this  :

 

  while (1)
  {

    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

		 HAL_GPIO_TogglePin(GPIOA, LED_1_Pin);
		 HAL_Delay(2000);
		 HAL_GPIO_TogglePin(GPIOA, LED_5_Pin);
		 HAL_Delay(2000);
		 HAL_I2C_IsDeviceReady(&hi2c1, 0xD0, 1, 1000);
  }
  /* USER CODE END 3 */
}

 

but this is the same, i just have 3.3V on I2C lines. I guess i was right and it might be an I2C settings issue. Im using the internal clock of STM32 could it be the problem ?

 

i show you the I2C code auto generated by CubeIDE

static void MX_I2C1_Init(void)
{

  /* USER CODE BEGIN I2C1_Init 0 */

  /* USER CODE END I2C1_Init 0 */

  /* USER CODE BEGIN I2C1_Init 1 */

  /* USER CODE END I2C1_Init 1 */
  hi2c1.Instance = I2C1;
  hi2c1.Init.Timing = 0x40000A0B;
  hi2c1.Init.OwnAddress1 = 0;
  hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
  hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
  hi2c1.Init.OwnAddress2 = 0;
  hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
  hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
  hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
  if (HAL_I2C_Init(&hi2c1) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Analogue filter
  */
  if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Digital filter
  */
  if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN I2C1_Init 2 */

  /* USER CODE END I2C1_Init 2 */

}

It isn't clear how you're seeing 3.3V, so are you using a oscilloscope to see if there is data activity and not just using a DMM?

Is this a custom board or a Nucleo/Discovery and MPU6050 board? Which STM32F4xx?

In either case, show how the MPU6050 is connected to the STM32 with pull-ups and values.

Upload your IOC file or better yet, upload the project.

 

 

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

I see that with an oscilloscope. I will try to show you my IOC file. But i just notice that my I2C lines are tied to 3.3V even if i disable I2C in IOC file ^^' i guess this is a hardware problem i will check that.