cancel
Showing results for 
Search instead for 
Did you mean: 

"Failed to execute MI command ...error from the debuggers end"

Harumoto_2
Associate II

i'm using Stm-Cube ide version 1.15.0 and getting this error when trying to flash the firmware.

Harumoto_2_0-1725535213578.png

 

4 REPLIES 4
TDK
Super User

Can you connect using the standalone STM32CubeProgrammer program?

What does test.elf do? If it goes into low power modes, or re-initialized SWD pins, or erases FLASH, this will cause issues with debug.

Is this a known good ST board or custom hardware?

If you feel a post has answered your question, please click "Accept as Solution".

it is a nucleo board-L452RET6

And the answers to the other questions?

If you feel a post has answered your question, please click "Accept as Solution".

sorry for the late reply. 
https://community.st.com/t5/stm32-mcus-products/quot-failed-to-execute-mi-command-load-failed-ltdc-paint-elf/td-p/94809
this helped me to clear the error 
Thanks for the reply