2019-11-21 6:43 AM
I'm monitorating heart rate by the MAX30100(https://img.filipeflop.com/files/download/Datasheet_MAX30100.pdf) using the MCU STM32F4. I'm trying read the IR and RED data from the FIFO, but all returns are **ZERO**. The method `MAX30100_Get_Num_Samples()` returns **8**. I modeled the code using the pseudo code from datasheet of MAX30100. I tried several solutions for my problem but doesn't work. I dont know if i'm following the right way to get data from the FIFO. My code:
I2C_HandleTypeDef hi2c3; //i2c used
uint16_t RED[50] = {0}, IR[50] = {0}; //buffers for RED and IR
uint8_t buffOximeter[5];
char buffer[32];
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C3_Init();
MX_USB_DEVICE_Init();
MAX30100_Init();
while (1)
{
uint8_t numSamples = MAX30100_Get_Num_Samples();
MAX30100_Read_HeartBeat(numSamples);
for(int i = 0; i < numSamples; i++)
{
sprintf(buffer, "Amostra %d: %d / %d\n\r", i , IR[i], RED[i]);
CDC_Transmit_FS((char*)buffer, 50);
}
}
}
static void MX_I2C3_Init(void)
{
hi2c3.Instance = I2C3;
hi2c3.Init.ClockSpeed = 400000;
hi2c3.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c3.Init.OwnAddress1 = 0;
hi2c3.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c3.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c3.Init.OwnAddress2 = 0;
hi2c3.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c3.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c3) != HAL_OK)
{
Error_Handler();
}
}
void MAX30100_Init(void)
{
HAL_I2C_Mem_Write(&hi2c3,0xAE,0x06,1,0x02,1,1000); //set heart rate mode
HAL_I2C_Mem_Write(&hi2c3,0xAE,0x09,1,0xFF,1,1000); //i50 ledCurrent
uint8_t sr = 0x01, pw = 0x3;
HAL_I2C_Mem_Write(&hi2c3,0xAE,0x07,1,(sr<<2)|pw,1,1000); //sr100, pw1600
HAL_Delay(50);
}
void MAX30100_Read_HeartBeat(uint8_t num)
{
for(int i=0;i<num;i++)
{
HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAE,1,1000); //adress + write mode
HAL_I2C_Master_Transmit(&hi2c3,0x57,0x02,1,1000); //send fifo_wr_ptr
HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAF,1,1000); //adress + read mode
uint8_t data;
HAL_I2C_Master_Receive(&hi2c3,0x57,&data,1,1000); //read fifo_wr_ptr
HAL_Delay(100); //STOP
HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAE,1,1000); //adress + write mode
HAL_I2C_Master_Transmit(&hi2c3,0x57,0x05,1,1000); //send adress fifo data
HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAF,1,1000); //adress + read mode
HAL_I2C_Mem_Read(&hi2c3,0x57,0x05,1,&buffOximeter,4,1000); //read fifo data
IR[i] = (buffOximeter[0] << 8) | buffOximeter[1];
RED[i] = (buffOximeter[2] << 8) | buffOximeter[3];
HAL_Delay(100); //STOP
HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAE,1,1000); //adress + write mode
HAL_I2C_Master_Transmit(&hi2c3,0x57,0x04,1,1000); //send adress fifo_rd_ptr
HAL_Delay(100);
}
}
int MAX30100_Get_Num_Samples(void)
{
uint8_t wrPtr, rdPtr;
HAL_I2C_Mem_Read(&hi2c3,0x57,0x02,1,&wrPtr,1,1000);
HAL_Delay(50);
HAL_I2C_Mem_Read(&hi2c3,0x57,0x04,1,&rdPtr,1,1000);
HAL_Delay(50);
return (abs( 16 + wrPtr - rdPtr ) % 16);
}
2019-11-21 7:14 AM
Hi @FFern.1463 , I suggest you to post the same question on the STM32 community page and/or on Maxim Q&A page, being the MAX30100 a Maxim sensor. Regards
2019-11-21 2:49 PM
What kind of forum software are you running? Just move posts to the appropriate sub-forum..
2019-11-22 3:15 AM
It is just a matter of editing tags (topics), I did it.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-11-22 4:07 AM
Thanks