cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4 UCPD:Debug issue

Susu
Associate II

Hello, 

I have encountered a similar problem to the one in this link .

I am also trying to use the UCPD Monitor to send message. For example, I request a new voltage from the source using the "Request Power Profile" message from the "Message Selector" , and I always get "Message rejected for this port configuration". 

After some investigations ,I find out that the USBPD_PE_Send_Request() function in the  USBPD_DPM_RequestMessageRequest() function is not working. It returns USBPD_OK the first time I use this function to request another fixed voltage PDO(9V),but actually it is not working. And when I use it again , it returns USBPD_BUSY. Besides, if I request the APDO, it returns USBPD_ERROR.

USBPD_StatusTypeDef USBPD_DPM_RequestMessageRequest(uint8_t PortNum, uint8_t IndexSrcPDO, uint16_t RequestedVoltage)
{
  USBPD_StatusTypeDef _status = USBPD_ERROR;
  uint32_t voltage, allowablepower;
  USBPD_SNKRDO_TypeDef rdo;
  USBPD_PDO_TypeDef  pdo;
  USBPD_CORE_PDO_Type_TypeDef pdo_object;
  USBPD_USER_SettingsTypeDef *puser = (USBPD_USER_SettingsTypeDef *)&DPM_USER_Settings[PortNum];
  USBPD_DPM_SNKPowerRequestDetails_TypeDef request_details;
  rdo.d32 = 0;

  /* selected SRC PDO */
  pdo.d32 = DPM_Ports[PortNum].DPM_ListOfRcvSRCPDO[(IndexSrcPDO - 1)];
  voltage = RequestedVoltage;
  allowablepower = (puser->DPM_SNKRequestedPower.MaxOperatingCurrentInmAunits * RequestedVoltage) / 1000U;

  if (USBPD_TRUE == USBPD_DPM_SNK_EvaluateMatchWithSRCPDO(PortNum, pdo.d32, &voltage, &allowablepower))
  {
    /* Check that voltage has been correctly selected */
    if (RequestedVoltage == voltage)
    {
      request_details.RequestedVoltageInmVunits    = RequestedVoltage;
      request_details.OperatingCurrentInmAunits    = (1000U * allowablepower)/RequestedVoltage;
      request_details.MaxOperatingCurrentInmAunits = puser->DPM_SNKRequestedPower.MaxOperatingCurrentInmAunits;
      request_details.MaxOperatingPowerInmWunits   = puser->DPM_SNKRequestedPower.MaxOperatingPowerInmWunits;
      request_details.OperatingPowerInmWunits      = puser->DPM_SNKRequestedPower.OperatingPowerInmWunits;

      DPM_SNK_BuildRDOfromSelectedPDO(PortNum, (IndexSrcPDO - 1), &request_details, &rdo, &pdo_object);

      _status = USBPD_PE_Send_Request(PortNum, rdo.d32, pdo_object);
    }
  }
  DPM_USER_DEBUG_TRACE(PortNum, "build rdo! _stauts = %d",_status);
/* USER CODE END USBPD_DPM_RequestMessageRequest */
  DPM_USER_ERROR_TRACE(PortNum, _status, "REQUEST not accepted by the stack");
  return _status;
}

Susu_0-1741242599589.png

Susu_1-1741242623726.png

 

 

5 REPLIES 5
FBL
ST Employee

Hi @Susu 

Thank you for reporting the issue.

Are you using G474 Nucleo + X nucleo DRP? Would you attach a minimum project to reproduce on my end?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
Susu
Associate II

Thanks for your reply, @FBL!

I'm not using the X nucleo DRP. The hardware Structure I am using now is roughly as follows:

Susu_0-1741742335442.png

The INA219 is used to monitor the VBUS voltage and current.

And the project is attached below.

Susu
Associate II

Sorry, the project above is not configured with three SNK PDOs

RJain.1
Associate III

Hi @Susu , 

Were you able to implement the complete SINK application? 

I am facing an issue with SRC PDO selection in cubemonitor.

Explicit contract has done correctly but unable to select a source PDO.

RJain1_0-1743701322440.png

 

Do you have any solution for it!

FBL
ST Employee

Hi @Susu 

I couldn't reproduce on my hardware setup (using X nucleo DRP).

First, check if the first request is completed. The USBPD_BUSY indicates that a request is already ongoing. This can happen if the first request did not complete successfully.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL