2020-02-14 2:22 AM
"Programmer To Go"
2020-02-14 2:52 AM
That would require the programmer pod to store the firmware file, which is much easier for Pic16/18 with their little Flash (<64k).
Besides of pricey industrial multi-gang programmers, I know no low-cost JTAG pods for Cortex M with that feature.
2020-02-14 3:20 AM
A Raspberry PI with OpenOCD can talk directly to SWD, so you can use it as a programmer as long as the target voltage is 3.3V
https://learn.adafruit.com/programming-microcontrollers-using-openocd-on-raspberry-pi
If the target voltage is different, you can still use a real ST-Link with the Pi (or build a voltage converter).
Then you can connect a few buttons and status LEDs to the spare pins on the Pi for headless operation, needing just a USB charger or power bank to work.
2020-09-10 1:54 PM
There were some commercial stand-alone/offline programmers available, but unfortunately all are not available.
Evo Primer (STM32PRIM-LAB): https://www.newark.com/stmicroelectronics/stm32prim-lab/dev-board-stm32-evoprimer-monitor/dp/06X3690
Cyclone / Cyclone FX: http://www.pemicro.com/partners/index.cfm?manufacturer_id=4
But you can still buy some interesting offline programmers on aliexpress - useful for field programming, but it is not exactly what you want.
https://www.aliexpress.com/i/32892646424.html