cancel
Showing results for 
Search instead for 
Did you mean: 

I have been using Microchip products with a PICKit3 programmer to program the new device firmware in the field using the "Programmer To Go" feature of MPLAB. Is there anything like this for STM32?

Graham1904
Associate III

"Programmer To Go"

3 REPLIES 3
Ozone
Lead III

That would require the programmer pod to store the firmware file, which is much easier for Pic16/18 with their little Flash (<64k).

Besides of pricey industrial multi-gang programmers, I know no low-cost JTAG pods for Cortex M with that feature.

berendi
Principal

A Raspberry PI with OpenOCD can talk directly to SWD, so you can use it as a programmer as long as the target voltage is 3.3V

https://learn.adafruit.com/programming-microcontrollers-using-openocd-on-raspberry-pi

If the target voltage is different, you can still use a real ST-Link with the Pi (or build a voltage converter).

Then you can connect a few buttons and status LEDs to the spare pins on the Pi for headless operation, needing just a USB charger or power bank to work.

Roman Priesol
Associate II

There were some commercial stand-alone/offline programmers available, but unfortunately all are not available.

Evo Primer (STM32PRIM-LAB): https://www.newark.com/stmicroelectronics/stm32prim-lab/dev-board-stm32-evoprimer-monitor/dp/06X3690

Cyclone / Cyclone FX: http://www.pemicro.com/partners/index.cfm?manufacturer_id=4

But you can still buy some interesting offline programmers on aliexpress - useful for field programming, but it is not exactly what you want.

https://www.aliexpress.com/i/32892646424.html

https://www.aliexpress.com/item/4000134196087.html

https://id.aliexpress.com/item/32978703795.html