cancel
Showing results for 
Search instead for 
Did you mean: 

I have a problem on debugging Nucleo-f446re

AAbde.8
Associate II

Failed to execute MI command:

target remote localhost:61234

Error message from debugger back end:

localhost:?????: No such file or directory.

localhost:?????: No such file or directory.

5 REPLIES 5

Perhaps be specific about the version of Windows and that of CubeIDE or whatever you're using.

Any kind of firewall or anti-virus that might block socket connections?

Tools installed whilst running as an Administrator?

Need better contextual understanding of what the situation is.

Looks like the GDB Server is not functioning.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AAbde.8
Associate II

I am using STM cubeide version 1.11.2 on windows 10 when i creat a project it is working without a problem if i closed the ide and open it again the problem occur

AAbde.8
Associate II

0693W00000aJbgfQAC.jpg

I am using STM cubeide version 1.11.2 on windows 10 when i creat a project it is working without a problem if i closed the ide and open it again the problem occur

this a photo for the error0693W00000aJbgfQAC.jpg

Fixed in second thread, switch Windows numeric from Arabic to English notation

https://community.st.com/s/question/0D53W00002CQxRySAL/i-have-a-problem-on-the-debugging

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..