2020-01-12 10:39 PM
2020-01-12 11:13 PM
You don't need to do anything particular in the UART, just change the Tx pin's setting in respective GPIO_MODER to GPIO_Output, perform the operation you want, and then change it back to AF.
JW
2020-01-13 1:09 AM
Many thanks. I go it to work. HAL_UART2_Init() after the GPIO toggling?
2020-01-13 1:42 AM
I don't use Cube/HAL, but I don't see the reason to do so.
JW
2020-01-13 2:12 AM
Surely you must re-configure the UART2?
2020-01-13 6:50 AM
i don't see any reason why you would need to reconfigure it, you only mess with the GPIO registers not usart periephal registers.
i believe that at most, messing with the GPIO, would toggle the TE(bit 3 -> Transmit enable) or UE(bit 0 -> usart enable) in USARTx_CR1 register, but you would have to confirm it with debugger. i suspect that it wont do anything to usart registers in the end, and simple changing the GPIO back to Alternative function will make it work again.