2023-09-14 1:30 AM
Hello everyone ,
I have a Project where i wish to have a 8Mhz PWM pulse. For this i use the HRTIM timer at 4.9Ghz with a period of 600
I have my PWM output but it seems that i can't set 0% duty cycle ? in fact duty cycle seems to not work between 0% & 16% (96) .
I have read differents subjects where people are expericiencing the same issue .
https://community.st.com/t5/stm32-mcus-products/stm32f334-hrtim-with-bad-behavior/td-p/409531
https://stackoverflow.com/questions/69572777/stm32-hrtim-pwm-only-work-when-master-compare-is-70ns
it seems that its just not doable with HRTIM on ST MCUs..
Could someone confirm that having 8mhz PWM with 0% to 100% duty cycle is not achievable with ST MCUs
best regards
2023-09-14 4:13 AM - edited 2023-09-18 2:49 AM
Hello @PJFIXER
The best way to do this is to test it using all possible configurations.
Best regards.
II
2023-09-18 8:45 AM
Hello,
Indeed, I confirm this rule for HRTIM:
rm0440-stm32g4: "The high-resolution behavior is not supported for pulses narrower than 3 tHRTIM periods"
For an HRTIM running at the max frequency: (5.44Ghz/96)*3 = 170Mhz
This is normal while PADs in MCUs could not support a very high frequencies, except PADs with PHYs, but this means allocating specific PADs for timer, without alternating which is a limitation for a general purpose MCU.
Best regards.