How to wake up from stop mode with alarm A?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-04-20 9:37 PM
Hello,
I'm trying to wake up from stop 1 with the alarm A, and I was wondering if someone can help me with this.
Here is my code (I'm using HAL libraries first, the "easy" way base on the example ST gives: PWR/STOP1_RTC):
...
int main(void){
GPIO_InitTypeDef GPIO_InitStruct;
HAL_Init();
BSP_LED_Init(LED2);
SystemClock_Config(); //Config RCC
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI);
SystemPower_Config(); //Config the RTC ----> 19:50:00
setAlarmA(); // The alarm is set to: 19:51:00
while(1){
...
/* Disable all used wakeup source */
HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle);
/* Re-enable wakeup source */
HAL_RTCEx_SetWakeUpTimer_IT( ........?........);
/* Enter STOP 1 mode */
HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
} //End while (1)
} // End main
I don't know how to tell my STM that it will be woken up by the Alarm A (It goes there in the line I highlighted?) How do I do that?
My idea is to wake up the system at 19:51:00 and re-set the alarm A to: 19:52:00. In the alarmA callback, I wrote the following:
void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc){
setNewAlarmA();
}
I'm using the Nucleo Board STM32L476RG
Thank you very much for all the help.
- Labels:
-
Power
-
RTC
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-04-22 5:28 AM
RTC Alarm is not a timer per se. Alarm A/B uses the RTC EXTI18 external interrupt, so EXTI18 must be enabled on rising edge to wake from STOP mode, for the NVIC vector in the configuration. Don't use the HAL, no idea how it handles EXTIs, but I use alarm B for something similar. RTC must be running in STOP mode with LSE or LSI clock on.
Jack Peacock