How to use OpenOCD to program the STM32F469 Discovery Board?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 9:16 AM
Hello,
I am trying to program the ST Discovery Demo binary on the board. This is the pre-built file provided with STM32Cube_FW_F4_V1.16.0. I am calling OpenOCD like this:
cd STM32Cube_FW_F4_V1.16.0/Projects/STM32469I-Discovery/Demonstrations/Binary
$HOME/Ac6/SystemWorkbench/plugins/fr.ac6.mcu.externaltools.openocd.linux64_1.16.0.201708311556/tools/openocd/bin/openocd \-s $HOME/Ac6/SystemWorkbench/plugins/fr.ac6.mcu.debug_2.1.2.201709081530/resources/openocd/st_scripts \-s $HOME/Ac6/SystemWorkbench/plugins/fr.ac6.mcu.debug_2.1.2.201709081530/resources/openocd/scripts \-f st_board/stm32f469i_disco.cfg \-c 'program STM32469I-Disco_Demo_V1.2.0_FULL.hex verify reset exit'OpenOCD outputs the following:
Open On-Chip Debugger 0.10.0-dev-00004-gcef2a8c-dirty (2017-08-31-14:01)
Licensed under GNU GPL v2For bug reports, read http://openocd.org/doc/doxygen/bugs.htmlInfo : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWDadapter speed: 1800 kHzadapter_nsrst_delay: 100Info : clock speed 1800 kHzInfo : STLINK v2 JTAG v25 API v2 M v13 VID 0x0483 PID 0x374BInfo : using stlink api v2Info : Target voltage: 3.240473Info : Stlink adapter speed set to 1800 kHzInfo : STM32F469.cpu: hardware has 6 breakpoints, 4 watchpointscan't read 'ENABLE_LOW_POWER': no such variablein procedure 'program' in procedure 'init' called at file 'embedded:startup.tcl', line 473in procedure 'ocd_bouncer'Info : Stlink adapter speed set to 1800 kHzadapter speed: 1800 kHzcan't read 'ENABLE_LOW_POWER': no such variablein procedure 'program' in procedure 'reset' called at file 'embedded:startup.tcl', line 478in procedure 'ocd_bouncer' in procedure 'ocd_process_reset' in procedure 'ocd_process_reset_inner' called at file 'embedded:startup.tcl', line 248in procedure 'STM32F469.cpu' called at file 'embedded:startup.tcl', line 299in procedure 'ocd_bouncer'STM32F469.cpu: target state: haltedtarget halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x080aeb28 msp: 0x20002c50configuring PLLInfo : Stlink adapter speed set to 1800 kHzadapter speed: 1800 kHz** Programming Started **auto erase enabledInfo : device id = 0x10006434Info : flash size = 2048kbytesSTM32F469.cpu: target state: haltedtarget halted due to breakpoint, current mode: Thread xPSR: 0x61000000 pc: 0x20000046 msp: 0x20002c50Warn : no flash bank found for address 90000000wrote 786432 bytes from file STM32469I-Disco_Demo_V1.2.0_FULL.hex in 25.377024s (30.264 KiB/s)** Programming Finished **** Verify Started **STM32F469.cpu: target state: haltedtarget halted due to breakpoint, current mode: Thread xPSR: 0x61000000 pc: 0x2000002e msp: 0x20002c50STM32F469.cpu: target state: haltedtarget halted due to breakpoint, current mode: Thread xPSR: 0x61000000 pc: 0x2000002e msp: 0x20002c50Error: checksum mismatch - attempting binary comparediff 0 address 0x90000000. Was 0x00 instead of 0x99diff 1 address 0x90000001. Was 0x00 instead of 0xa5*** LOTS OF THESE ****** LOTS OF THESE ***diff 127 address 0x9000007f. Was 0x00 instead of 0xa5More than 128 errors, the rest are not printed.** Verify Failed **shutdown command invokedWhat am I doing wrong? Shouldn't this work?
#openocd #stm32f469i-disco- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-09 6:20 AM
I'm getting a very similar problem trying to load what I think is the default firmware to the STM32F769UI-DISCO.
When I rebuild the application in Eclipse with STM32 workbench I get that same verification error. By manually pressing the reset button the discovery board boots and the example firmware is running but all of the graphics are scrambled.
Loading using external tools (gdb / openocd) I don't get errors but the graphics are still scrambled. It seems like something in the memory management is incorrect, do the graphics need to be loaded to the off-chip memory instead somehow?
How to return the Discovery board to its factory state?
James
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-10 12:42 PM
,
,
In case you get this:
Warn : no flash bank found for address 90000000
Parts of the firmware (in particular bitmaps) are located in the external spi flash, not in the controllers internal flash. To program/erase the external spi flash as well, you need the patch openocd, see
http://openocd.zylin.com/ ♯ /c/4321/
,- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-11 5:48 PM
Good info. Thanks.
James