cancel
Showing results for 
Search instead for 
Did you mean: 

How to reduce the project size.

hello
Associate II
Posted on June 23, 2012 at 20:56

hi,

i have the project from IAR Embedded workbench when i try to compile it size code exceed,, i am using only code size limited.

this project have lot of function like LCD, Temp sensor, USART, ect..

now i am just trying to use only USART and CAN function..

so how i can remove those unwanted function from that project.

Thanks.....
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on June 23, 2012 at 23:47

Edit the files to remove the unused/unwanted functions?

(or disable them with #if)

If complete files are unused, remove them from the project?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
hello
Associate II
Posted on June 24, 2012 at 00:30

thanks for your reply..

i remove some file which i dont want to use then i got like

Error[Li005]: no definition for ''Stepper_Motor_Test'' [referenced from C:\Documents and Settings\RAJ\Desktop\ST\STM32F10x\IAR-STM32F107VC-SK\Test_Demo\project\EWARMv5\STM32F107VCT6\Obj\menu.o] 

i got some of the error like this what i can do for such error.
Posted on June 24, 2012 at 01:48

Remove calls to functions and files you have removed.

Alternatively start a new project and just copy in the functionality you want/need. The firmware library contains template projects which are empty, copy these to new directories.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..