2021-02-10 01:24 AM
Hi, i need to measure rms voltage and current choosing ADC channels in stm32f103.
i selected two channnels in ADC1 to read adc values . By using these channels i need to calculate rms voltage and current . But i am confused how to do it . is it necessary to do calibration also. can anyone help me how to write a code or how to start it please.
Thank you
Solved! Go to Solution.
2021-02-10 03:58 AM
True RMS calculation:
1.Detect the 0 crossing (here is where the magic is)
2. offset your adc readings tothat 0
3. calculate the root square of every sample and average the results.
(the more samples you get the more precise your result is)
Cheap-fix RMS calculation:
if your signal is going to have a very stable dc component (same average all the time) you can just make a peak detector and do Vrms=(1/sqrt2)*(Vmax-Vavg)
2021-02-10 02:41 AM
Hello @Lchal.1 ,
The current can be measured through a resistor: by measuring the voltage across this resistor.
The RMS is an average, so it must average the values taken by the ADC by software.
Perhaps I did not understand your question.
So, I suggest adding more details and clarify your request to increase the chances of getting you an answer.
Imen
2021-02-10 03:47 AM
Thank you
2021-02-10 03:53 AM
if(HAL _ADC _Start _DMA(&hadc1, (uint32_t*) adc Buffer, TOTAL_CHANNELS) != HAL_OK)
return 0;
if(RMS _Sample_ Counter<RMS_TOTAL_SAMPLES) // it is given inside timer interrupt by setting 1kz
{
for(index1=0;index1<2;index1++)
{
temp_ ADC = adc Buffer[index1];
V1[index1] = V1[index1]+((float)temp _ADC*(float)temp _ADC);
V2[index1] = V2[index1]+(float)temp _ADC;
}
RMS _Sample _Counter++;
}
while(1)
{
Delay_Count++;
if(Delay_Count>=2500)
{
Delay_Count = 0;
if(RMS_Sample_Counter>=RMS_TOTAL_SAMPLES) // i have set RMS_TOTAL_Samples as 1000
{
for(indx=0;indx<2;indx++)
{
//RMS_value[indx] = ((sqrtf((V1[indx]/100000.0)-((V2[indx]/100000.0)*(V2[indx]/100000.0))))/15.5);
RMS_value[indx] = ((sqrtf((V1[indx]/1000.0)-((V2[indx]/1000.0)*(V2[indx]/1000.0))))/caliberate_factor);
if(RMS_value[indx]>1.5)
{
Actual_Amps[indx] = RMS_value[indx];
}
else
{
Actual_Amps[indx] = 0.0;
}
/*
for(indx=0;indx<3;indx++)
{
//Amps_Reading[indx] += 0.1;
if(Amps_Reading[indx]>30)
{
Amps_Reading[indx] = 0;
}
Actual_Amps[indx] = Amps_Reading[indx];
}
*/
V1[indx] = 0;
V2[indx] = 0;
}
RMS_Sample_Counter = 0;
}
}
}
this is the code i have done to calculate rms voltage and current can anyone help me if anything i need to add or is my code correct please
Thank you
2021-02-10 03:58 AM
True RMS calculation:
1.Detect the 0 crossing (here is where the magic is)
2. offset your adc readings tothat 0
3. calculate the root square of every sample and average the results.
(the more samples you get the more precise your result is)
Cheap-fix RMS calculation:
if your signal is going to have a very stable dc component (same average all the time) you can just make a peak detector and do Vrms=(1/sqrt2)*(Vmax-Vavg)