2019-01-12 3:57 AM
I am going to use STM32F030k6t6. IC is not having VBAT pin. Please suggest how to make RTC active when power is off
2019-01-12 7:47 AM
The 'F030 is a cut-down version of the 'F031/'F051, with some features deliberately left off.
In other words, you have to chose an STM32 model which has the VBAT pin.
JW
2019-01-13 8:38 PM
Dear Waclawek.jan sir,
Thanks for your reply .
I want to know is there any solution to use stm32f030k6t6 as clock. As i want to make cost effective application.
2019-01-14 12:08 AM
You can have an external switchover (maybe just a diode or two) from primary power source to battery, and write the software so that if primary source goes away the mcu goes into some of the low-power mode.
However, the battery consumption will be higher than it would be using a mcu with VBAT pin.
jW
2019-01-14 1:37 AM
Please share the details or link about how to deal with low power modes for respective microcontroller. it will be very helpful for me
2019-01-15 2:18 PM
Isn't STM32L010K4 or similar chips more appropriate, if energy consumption and low power modes are important? The price is approximately the same. Are there some other special requirements?