cancel
Showing results for 
Search instead for 
Did you mean: 

How to fix ST-Link Nucleo board unable to connect, where the target is not found and the st-link is showing chipid 0x0000

JMora.7
Associate II

Hello I ordered two NUCLEO boards, to start some projects on the ST32G03 platform. I was using the board with out an issue and connected to am Ubuntu 20.04 sys, updated the firmware on both and now one is working and the other is not, here is an output from dmesg inserting one then the other.

Device= 1.00
[108303.597126] usb 1-5: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[108303.597131] usb 1-5: Product: STM32 STLink
[108303.597134] usb 1-5: Manufacturer: STMicroelectronics
[108303.597138] usb 1-5: SerialNumber: 066EFF3933354D5043113431
[108303.657933] usb-storage 1-5:1.1: USB Mass Storage device detected
[108303.658528] scsi host1: usb-storage 1-5:1.1
[108303.659177] cdc_acm 1-5:1.2: ttyACM0: USB ACM device
[108304.684568] scsi 1:0:0:0: Direct-Access     MBED     microcontroller  1.0  PQ: 0 ANSI: 2
[108304.685186] sd 1:0:0:0: Attached scsi generic sg1 type 0
[108304.685833] sd 1:0:0:0: [sdb] 200 512-byte logical blocks: (102 kB/100 KiB)
[108304.686064] sd 1:0:0:0: [sdb] Write Protect is off
[108304.686074] sd 1:0:0:0: [sdb] Mode Sense: 03 00 00 00
[108304.686277] sd 1:0:0:0: [sdb] No Caching mode page found
[108304.686291] sd 1:0:0:0: [sdb] Assuming drive cache: write through
[108304.757126] sd 1:0:0:0: [sdb] Attached SCSI removable disk
[108384.531001] usb 1-5: USB disconnect, device number 60
[108384.546598] FAT-fs (sdb): unable to read boot sector to mark fs as dirty
[108395.017370] usb 1-5: new full-speed USB device number 61 using xhci_hcd
[108395.167110] usb 1-5: New USB device found, idVendor=0483, idProduct=374b, bcdDevice= 1.00
[108395.167122] usb 1-5: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[108395.167126] usb 1-5: Product: STM32 STLink
[108395.167130] usb 1-5: Manufacturer: STMicroelectronics
[108395.167132] usb 1-5: SerialNumber: 066EFF3933354D5043120830
[108395.225380] usb-storage 1-5:1.1: USB Mass Storage device detected
[108395.225889] scsi host1: usb-storage 1-5:1.1
[108395.226451] cdc_acm 1-5:1.2: ttyACM0: USB ACM device
[108396.233965] scsi 1:0:0:0: Direct-Access     MBED     microcontroller  1.0  PQ: 0 ANSI: 2
[108396.234247] sd 1:0:0:0: Attached scsi generic sg1 type 0
[108396.234597] sd 1:0:0:0: [sdb] 200 512-byte logical blocks: (102 kB/100 KiB)
[108396.234752] sd 1:0:0:0: [sdb] Write Protect is off
[108396.234755] sd 1:0:0:0: [sdb] Mode Sense: 03 00 00 00
[108396.234902] sd 1:0:0:0: [sdb] No Caching mode page found
[108396.234906] sd 1:0:0:0: [sdb] Assuming drive cache: write through
[108396.318817] sd 1:0:0:0: [sdb] Attached SCSI removable disk
[108425.954629] usb 1-5: USB disconnect, device number 61
[108425.971849] FAT-fs (sdb): unable to read boot sector to mark fs as dirty

the first one works great and the second one is not able to connect to the g03 board. Here is the output os the st-info probe.

This is from the working one. 
 
st-info --probe                                                                     
Found 1 stlink programmers
  version:    V2J34S25
  serial:     066EFF3933354D5043113431
  flash:      65536 (pagesize: 2048)
  sram:       8192
  chipid:     0x0466
  descr:      G030/G031/G041
 
This is from the failing one: 
st-info --probe
Found 1 stlink programmers
  version:    V2J35S26
  serial:     066EFF3933354D5043120830
  flash:      0 (pagesize: 0)
  sram:       0
  chipid:     0x0000
  descr:      unknown device

This failed only after the firmware upgrade, is there any way to revert this?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

You can use the firmware update tool to go to older versions, you just have to download the appropriate one.

V2J35 is still rather OLD

ST-LINK Firmware Update https://www.st.com/en/development-tools/stsw-link007.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
JMora.7
Associate II

Thank you for your recommendation, I could have sworn I tried that, but I have to double check, Any specific procedure I need to take to ensure this is done correctly? Thank you.

JMora.7
Associate II

Well, I tried going back to an older firmware and it did not work.

 st-info --probe
Found 1 stlink programmers
  version:    V2J38S27
  serial:     066EFF3933354D5043120830
  flash:      0 (pagesize: 0)
  sram:       0
  chipid:     0x0000
  descr:      unknown device
 
 
 
116658.613598] usb 1-5: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[116658.613603] usb 1-5: Product: STM32 STLink
[116658.613607] usb 1-5: Manufacturer: STMicroelectronics
[116658.613610] usb 1-5: SerialNumber: 066EFF3933354D5043120830
[116658.875053] usb-storage 1-5:1.1: USB Mass Storage device detected
[116658.875654] scsi host1: usb-storage 1-5:1.1
[116658.876542] cdc_acm 1-5:1.2: ttyACM0: USB ACM device
[116659.888859] scsi 1:0:0:0: Direct-Access     MBED     microcontroller  1.0  PQ: 0 ANSI: 2
[116659.889588] sd 1:0:0:0: Attached scsi generic sg1 type 0
[116659.890240] sd 1:0:0:0: [sdb] 456 512-byte logical blocks: (233 kB/228 KiB)
[116659.890532] sd 1:0:0:0: [sdb] Write Protect is off
[116659.890538] sd 1:0:0:0: [sdb] Mode Sense: 03 00 00 00
[116659.890881] sd 1:0:0:0: [sdb] No Caching mode page found
[116659.890889] sd 1:0:0:0: [sdb] Assuming drive cache: write through
[116659.953695] sd 1:0:0:0: [sdb] Attached SCSI removable disk