2020-07-06 4:50 AM
I am trying to establish an SPI connection using the Nucleo-F030R8 board but there's no signal coming out. How do you start the connection?
I did the configurations using STM32CUBE MX software and code it using TrueStudio. Is there any line of code apart from MX_SPI1_Init(); that is already automatically generated?
As for the pins I am sure it is not faulty as I tried to toggle each and they were visible in the logic analyzer but when I tried to send Data through SPI, even the clock doesn't get triggered.
is there a step that I missed in order for the clock to be triggered?
thanks for the help