2024-09-05 9:39 PM
Hello everyone.
I want to connect 8 SRAMs (2MB) to STM32H755XIH3 and use them as 16MB work memory.
When connecting 8 memories (SRAMs) using FMC (devices more than the number of FMC_NE*), how should I connect and control them? If there are any similar cases, I would appreciate your advice.
I am currently considering it, but I have some conditions.
1. I will use Infenion's CY7C1061GE30-10BVJXIT (2MB) with dual chip enable for the SRAM.
2. Of the 4 NEs in the FMC, 2 will be used to connect other memories, so only 2 can be used for SRAM.
Thank you in advance.
Solved! Go to Solution.
2024-09-06 3:32 AM - edited 2024-09-06 5:08 AM
@kazutobi wrote:
The SRAM I'm trying to use has two chip enable terminals.
I was thinking of doing it without a decoder. I don't know if that's possible though.
Two chip enable is to enable the memory itself. You need to use one and fix the another. You need as @Tesla DeLorean said an address decoder like the old TTL "74138" to address 8 memories. Each 74138 output will drive a chip enable of a memory. The address decoder is driven by the Higher address lines.
This is an old concept. So for example this link: https://ece-research.unm.edu/jimp/310/slides/8086_memory2.html
2024-09-08 10:13 PM
Hi LCE
Thank you very much.
I will consider whether HYPERRAM matches our system.
It is true that pattern design for 8 SRAM is troublesome.
Thank you for the useful information.
2024-09-08 10:23 PM
Hello
Thank you very much for the detailed explanation. And thanks for the link.
I understand that I need an address decoder, as @Tesla DeLorean told me.
I will continue to consider whether to go with 8 SRAMs or use the HYPERRAM that @LCE told me about.
2024-09-17 5:48 PM
I'm commenting because "Accept as Solution" is not displayed.
I accept your answer. Thank you.