cancel
Showing results for 
Search instead for 
Did you mean: 

How do LVDS displays connect to STM32H7, which has only RGB or MIPI-DSI outputs?

mtavazoei23
Associate

I'm using TouchGFX with an STM32H7, which provides RGB and MIPI-DSI interfaces but no native LVDS output.
Riverdi offers LVDS displays and even dev boards using STM32H7—how is the LVDS interface achieved in such cases?

 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @mtavazoei23, to the community!

You could take a look at this thread, which should answer your question.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.